Contact us

A new window will open A new window will open

Toshiba Launches New Generation Solid State Hybrid Drives

January 6, 2015

Solid State Hybrid Drives

Toshiba’s new SSHD series unleashes NAND capabilities, delivering capacity and speed
 

TOKYO— Toshiba Corporation’s (TOKYO: 6502) Semiconductor & Storage Products Company today announced the launch of its new solid state hybrid drive (SSHD) series, which is equipped with Toshiba's 19nm second-generation NAND flash memory. The new  ”MQ02ABD100H” SSHD offers 1TB[1] capacity in a drive 9.5mm high, while the  ”MQ02ABF050H” offers a capacity of 500GB in a 7 mm high form factor. Sample shipments will begin from February.
 

SSHDs deliver better performance compared to traditional hard disk drives (HDD), because the drives feature NAND that is used as the secondary cache during operation. This means users see improvement to the drive’s performance compared to traditional HDDs, while still maintaining the equivalent capacities of traditional HDDs.
 

The ”MQ02ABD100H” and ”MQ02ABF050H” are suitable for high-performance PCs like mainstream and gaming PCs, while the ”MQ02ABF050H”'s height of 7mm makes it suitable for ultra-thin and ultra-portable computing devices.
 

Toshiba’s new generation SSHDs merge the NAND controller function into the main HDD controller chip. This all-in-one system on chip (SoC) for the ”MQ02ABD/ABF-H” series enables more integrated management of the HDD and NAND operation compared to previous Toshiba SSHDs (”MQ01ABD-H” and ”MQ01ABF-H” series) that featured separate NAND and HDD controller chips. With its engineering expertise and experience, Toshiba combines its NAND, HDD and SSD technologies to develop and produce SSHDs. Toshiba’s NAND controller technologies unleash the NAND capabilities such as defective block management, ECC (Error Correction Code), conversion of logical block address and wear-leveling.
 

The new generation SSHDs also offer compatibility in both physical size and interface with traditional 2.5-inch HDDs. In other words, SSHDs allow for improved physical space efficiency within a system compared to alternatives that use a discrete SSD cache drive alongside an HDD. When using SSHDs, systems can access the drive through a single interface without the need for specific device driver software. Because it is a single unit, the SSHD is a lower cost alternative to SSDs while offering similar performance.
 

Notes:

[1] Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes.  A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1,073,741,824 bytes and therefore shows less storage capacity.  Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content.  Actual formatted capacity may vary.


 

Customer Inquiries:

Storage Products Division

Tel: +81-3-3457-2445

http://toshiba.semicon-storage.com/ap-en/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.