Contact us

A new window will open A new window will open

Toshiba Launches ApP Lite™ "TZ2100" Starter Kit

February 23, 2015

product photo:"RBTZ2100-1MA"

TOKYO – Toshiba Corporation (TOKYO: 6502) today announced the launch of two starter kits, RBTZ2100-1MA and RBTZ2100-2MA for development of applications using ApP Lite™ “TZ2100". Shipments are scheduled to start in March from Sohwa & Sophia Technologies*1.
 

The TZ2100 group supports enhanced audio and image data-mining, communications and security functions with a single-core ARM® Cortex® A9 core and a clock rate up to 600MHz. It is suitable for a wide range of applications, such as small embedded devices, handheld devices, industrial equipment and amusement equipment. Sample shipment started in December 2014.
 

The development starter kits include reference boards and device drivers that allow devices to be evaluated in their final application environment. This can reduce use of developer resources and shorten the development schedule.
 

*1 http://www.ss-technologies.co.jp/en/index.html

Main Features

  • Ability to evaluate function and performance, and advanced software development
  • The RBTZ2100-1MA can use Media I/F of camera, LCD panel while the RBTZ2100-2MA can use external bus I/F. Users can choose the suitable product depending on its required application.
  • Board Support Package ( BSP ) which supports Linux® and μ-ITRON is also provided for efficient software development.

Product Structure

  • Reference board, AC adapter cable, BSP, and user’s manual

Usage

  •  Advanced software and system development, applicable for various applications.

Product specifications

Hardware Specifications

Part number

RBTZ2100-1MA RBTZ2100-2MA
Applications general-purpose entertainment
Processor TZ2102 with ARM® Cortex®-A9 (Core clock:600MHz)
RAM 512MB DDR3L SDRAM 256MB DDR3 SDRAM
Flash ROM 16MB SPI Flash ROM 256MB Parallel Flash ROM
Audio

Mono microphone in,

Stereo headphone out

I2S connector
Camera Camera input connector (parallel) -
Touch panel LCD panel connector -
SD/MMC MicroSD Memory Card Slot×1
-
Extended interfaces


USB2.0 host/device(exclusive),

10/100 LAN connector

ADC connector

USB2.0 host

32bit external bus interface connector
e.g. UART, I2C, PWM, SPIM
JTAG ARM JTAG connector
Power supply DC5V

BSP

Part number

RBTZ2100-1MA RBTZ2100-2MA
OS Linux (Ubunts 14.04 Arm hf) µ-ITRON*2 -
Development environment gcc EWARM *3 EWARM
Boot loader U-boot Original Chain Loader Original Chain Loader
Supported device drivers

Ethernet,
UART,
SPIB,
I2C,
Audio,
GPIO,
SPIM,
USB(EHCI/OHCI),
e・MMC™,
Memory Allocator,

SD/SDIO

Ethernet,
UART,
SPIB,
I2C,
Audio,
GPIO,
SPIM,
USB(EHCI/OHCI),
e・MMC™,

SD/SDIO

UART,
I2C,
Audio,
GPIO,

SPIM

2  eForce Co., Ltd. : µC3 (Standard)

http://www.eforce.co.jp/products/microc3s

3 IAR Embedded Workbench®

https://www.iar.com/iar-embedded-workbench/

※ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere.

※Linux is a registered trademark of Linus Torvalds in the U.S. and other countries.

※e ·MMC is a trademark of JEDEC Solid State Technology Association.

※ApP Lite is a trademark of Toshiba Corporation.

※Other company name and product name are possibly each company uses as own trademark or registered trademark.

Please refer to the below website for more detailed information.

http://toshiba.semicon-storage.com/ap-en/product/assp/applite/tz2000.html

Customer Inquiries:

Logic LSI Sales & Marketing Group

Tel: +81-44-548-2110

http://toshiba.semicon-storage.com/ap-en/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.