Contact us

A new window will open A new window will open

Toshiba Expands Line-up of ARM® Cortex®-M0-based Microcontroller for MFPs and Printers

February 6, 2015

product photo:"TMPM036FWFG"

Increasing communication and timer function channels to optimize device selection
 

TOKYO – Toshiba Corporation (TOKYO: 6502) today announced the launch of a new microcontroller, "TMPM036FWFG", as the latest addition to its ARM® Cortex®-M0-based "TX00 series". The new IC, housed in LQFP100-pin package, is optimized for MFPs and printers. Sample shipments will start in March 2015.
 

In MFP and printer applications, the microcontroller needs to communicate with the main control unit and onboard peripherals units. It also needs to have a timer function that can output pulses to control stepping motors and DC motors. An increase in the number of channels is required in both functions, as the first step to developing more fully featured MFP and printers.
 

Housed in LQFP100-pin package, the "TMPM036FWFG" offers more communication and timer function channels than Toshiba’s current IC in volume production, the "TMPM037FWUG", which is housed in LQFP64-pin package. The new IC incorporates an 8-channel communication interface, two channels more than the current IC, and a 14-channel 16-bit timer against 10 channels in the "TMPM037FWUG". Developers can select the optimum microcontroller according to the system scale or usage from these two products.
 

TMPM036FWFG is an ARM® Cortex®-M-based microcontroller, allowing use of the same development environment system as for the current ARM® Cortex®-M-based TX03/TX04 series. This improves the cost-efficiency of system development.
 

Applications

  • MFPs and printers
  • Consumer electronics
  • Digital equipment
  • Industrial equipment

Key Features of New Product

  • CPU: ARM® Cortex®-M0; Maximum operating frequency 20 MHz.
  • Built-in 8-channel communication interface (6-channel SIO/UART; 2-channel I2C)
  • Built-in 14-channel 16-bit timer
  • LQFP100-pin package

Specifications

Part number TMPM036FWFG
Sample price (tax included) 400 yen

Main

specifications

CPU ARM® Cortex®-M0
Maximum frequency 20 MHz
Internal memory Flash 128 Kbytes
SRAM 16 Kbytes
Operating voltage 2.3 to 3.6 V
10-bit ADC 8 ch
DMA 2 units
16-bit timer 14 ch
SIO/UART 6 ch
I2C 2 ch
Package LQFP100 (14 mm × 14 mm, 0.5 mm pitch)
Note DMA: Direct Memory Access
1 Kbyte is calculated as 1024 bytes.
For more information about the products, please visit:

http://toshiba.semicon-storage.com/info/lookup.jsp?pid=TMPM036FWFG&region=apc&lang=en

For more information about Toshiba ARM core-based microcontrollers, please visit:

http://toshiba.semicon-storage.com/ap-en/product/microcomputer/lineup/arm-micon.html

* ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere.

Customer Inquiries:

Mixed Signal IC Sales and Marketing Department

Tel: +81-44-548-2241

http://toshiba.semicon-storage.com/ap-en/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.