Contact us

A new window will open A new window will open

Toshiba Expands Line-up of ApP Lite™ Processor Family for IoT Solutions

September 4, 2015

product photo:"TZ1041MBG"

– The new sensor hub IC with Bluetooth® v4.1 –
 

TOKYO – Toshiba Corporation (TOKYO: 6502) today announced the launch of "TZ1041MBG", an application processor for wearable devices, the latest addition to its ApP Lite™ family TZ1000 series of solutions for the Internet of Things (IoT), first released in March 2014. Sample shipments will start in October and mass production is scheduled for January 2016.
 

The TZ1041MBG meets the increasing market demand for IoT devices that can support multiple external sensors, providing a versatile communication environment that makes use of the extended hub features of Bluetooth.
 

The new processor incorporates a Bluetooth v4.1 controller and processor, capable of capturing data from external sensors connected via various I/Os, such as I2C, UART, SPI and ADC, and it also incorporates flash memory to save data.
 

Data processing and storing of multiple sensing targets required for IoT devices are executable simultaneously by the new processor. In addition, TZ1041MBG can perform as a Bluetooth hub for collecting, processing and storing data, while its automatic reconnection function improves the operating efficiency and usability of the user system by using Low Duty Cycle Directed Advertising[Note].
 

Like other TZ1000 series devices, TZ1041MBG integrates a low power design feature that allows it to change supply voltage in response to the processor frequency. This makes it suitable for wearable products that require long operating hours.
 

Toshiba also supports sophisticated software algorithms for TZ1000 series, such as Activity Monitoring, PPG (Photoplethysmography) Monitoring and ECG (electrocardiography) Monitoring, which provides a total system solution for wearable products.
 

Key Features

Bluetooth v4.1 compliant

Integration of Bluetooth Smart controller and RF circuit allows transfer of raw and processed data to external devices, such as smartphones and tablets, enables:

  • Data collection, processing and storage, as a hub for Bluetooth communication devices
  • Low Duty Cycle Directed Advertising with automatic reconnection function
Low power design

Significantly reduces power consumption during operation; suitable for long hours of collecting and monitoring data as a sensor hub.

Communication function, memory and processor integrated in one package

Functions required for IoT devices are integrated into a single package, securing smaller system design.

Embedded ARM® Cortex®-M4F processor

The high performance ARM Cortex-M4F with DSP and floating point processing unit can collect  and process data from multiple external sensors.

High resolution ADCs

Integrates a 24-bit high resolution ΔΣADC with high speed switches connecting to three input channels. Capable of meeting the challenge of accurately measuring biomedical signals, such as the pulse and the heart’s electrical signal.

Applications

Wearable devices, such as activity monitoring products, smart watches, bracelet and glasses-type devices, and IoT devices.

Product Lineup

Product Name TZ1021MBG TZ1031MBG TZ1011MBG TZ1041MBG
CPU ARM Cortex-M4F
Maximum frequency 48MHz
SRAM 288KB
Storage embedded NOR flash memory 8Mbit

Sensor

(number of sensor)

Accelerometer

- -
Gyroscope - -
Magnetometer - - -
Bluetooth Core Specification Version - 4.0 4.1
Bluetooth Smart -
24bit delta-sigma ADC 3 ch
I/O USB USB 2.0
SPI 4 ch
I2C 3 ch
UART 3 ch

Dimensions

W×D×H mm
6.70×4.00×1.00 8.50×9.80× 1.60 6.70×8.00×1.59
Engineering Sample Available Oct. 2015
Mass Production Available Jan. 2016

Note: Low Duty Cycle Directed Advertising: a new function supported by Bluetooth ver. 4.1 that enables automatic reconnection when a known device comes within the communication area covered by a hub.
 

* Bluetooth is a registered trademark owned by Bluetooth SIG, Inc. and any use of such mark by Toshiba is under license.

* ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere.

* ApP Lite is a trademark of Toshiba Corporation.

* All other trademarks and trade names are properties of their respective owners.

For further information about this product, please visit:

http://toshiba.semicon-storage.com/ap-en/product/assp/applite/tz1000.html

Customer Inquiries:

Logic LSI Sales & Marketing Group

Tel: +81-44-548-2110

http://toshiba.semicon-storage.com/ap-en/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.