Contact us

A new window will open A new window will open

Toshiba’s Electrostatic Discharge (ESD) Protection Device with 0.13μm Process for Analog Power Semiconductor Improves ESD Characteristics

June 15, 2016

TOKYO—Toshiba Corporation (TOKYO: 6502) has developed an electrostatic discharge (ESD) protection device for analog power semiconductor application, fabricated with advanced 0.13μm process technology, that optimizes the structure of transistor and significantly improves ESD characteristics. ESD protection is much more robust, up four times, and the standard deviation is only 1/12 that of the conventional structure. Analysis of 3D simulations has also allowed Toshiba to identify a mechanism for optimizing transistor structure to boost ESD robustness. Toshiba announced these advances at “ISPSD2016”, the international semiconductor symposium held in Czech on June 14, 2016.

Injections of ESD surges, whether from the human body or equipment, have the potential to destroy semiconductor devices, as ESD current flows cause local temperature increases inside silicon. ESD protection devices are required to protect internal circuit. This is especially true for analog power semiconductor devices required to apply 10V to 100V, which need a high rated voltage. In this case, ESD protection devices must ensure high current flow, which results in enlarged chip size. Shrinking the size of the ESD protection device is an issue in realizing more compact chips.

Using 3D simulation analysis of an ESD event, Toshiba found out that ESD induced destruction is caused by lattice temperature increase due to the current flowing at the highest electric field point. Modifying the transistor structure, which extending the drain low resistive region to the source direction and suppressing the lateral silicon resistance, shifts the current flow from the bottom of the drain to source direction and detaches it from the highest electrical field point. This optimized design was found to increase ESD robustness by up to four times and to decrease the standard deviation down to 1/12. In addition, the device size required to ensure HBM* ±2000V was cut by 68%.

Toshiba offers advanced analog process platforms, with 0.13μm process technology, that can be embedded with the transistors such as CMOS, DMOS, bipolar transistor and the passive devices such as resistor and capacitor. User can select a process suited to each application from three process platforms: “BiCD-0.13” is mainly for automotive (DMOS line up is up to 100V); “CD-0.13BL” is mainly for motor control drivers (DMOS line up is up to 60V); and “CD-0.13” process is mainly for power management IC (DMOS line up is up to 40V).

Toshiba plans to release products using the CD-0.13 process applied in this technology in 2017 and proactively continue to implement to other process platforms to improve electrostatic discharge characteristics.

* HBM (Human Body Model) : one of the parameter to indicate ESD robustness

Schematic cross-section of studied structure.
Fig.1 Schematic cross-section of studied structure.

3D-Simulation results for studied structure.
Fig.2 3D-Simulation results for studied structure.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.