Contact us

A new window will open. A new window will open.

Bright Mode

Bright mode allows you to capture videos at high frame rates and yet delivers image brightness up to four times higher than Normal mode. By adopting interlaced scan, Bright mode delivers Full HD videos at 240 frames per second (fps) equivalent. Toshiba offers state-of-the-art video technologies necessary to realize high-frame-rate video capturing with outstanding picture quality, which makes for smooth slow playback.

Requirements and Challenges for Realizing High-Frame-Rate Videos

Effects of Frame Rates on Video Quality in Slow Motion

Slow motion can be realized when a video is played back at a rate slower than that at which it was captured. The more frames per second, the smoother the video will be when replayed in slow motion. Therefore, a high frame rate is desirable when capturing a fast-moving object.

Suppose, for example, that you capture a moving object at 60 fps and 240 fps and then replay the two versions of the video at 30 fps. When a video captured at 60 fps is replayed at 30 fps, the flow of images appears to be jumpy. The video captured at 240 fps has four times as many frames per second as the one captured at 60 fps and thus plays back more smoothly.

 Captured at 60 fps→Replayed at 30 fps:Fewer frames lead to jumpy motion. Captured at 240 fps→Replayed at 30 fps:More frames lead to smooth motion.

Challenges for Realizing High-Frame-Rate Videos

The more frames captured per second, the shorter the exposure time per frame and the darker the image will be. Therefore, an innovative technology was necessary to realize high picture quality and high frame rates simultaneously.

The more frames captured per second, the shorter the exposure time per frame.

Bright Mode Technology

You need Flash player 8+ and JavaScript enabled to view this video.

Bright Mode Features

Delivers images with up to four times the brightness and doubles the frame rate compared with normal mode

Bright mode quadruples image brightness by using a charge binning method to double the brightness of each pixel and by securing twice the exposure time for each frame. Additionally, use of the interlaced output doubles the frame rate. These techniques combine to realize bright video capturing at high frame rates.

Charge binning: 2× brightness
Charge binning adds the charges of two pixels and outputs the sum as one pixel with double brightness.

This figure shows charge binning: 2× brightness.

Interlaced output: 2× frame rate
The most commonly used scanning method for CMOS sensors is progressive scan in which all the lines of each frame are output in sequence. In contrast, Bright mode uses interlaced scan in which only the odd lines of each frame, and then the even lines, are output alternately, doubling the frame rate.

This figure shows interlaced output: 2× frame rate.

Exposure time for two consecutive frames: 2× brightness
Interlaced scan makes it possible to extend the exposure time up to the length of two consecutive frames. Therefore, it delivers video capturing with up to twice the exposure time for each frame.

This figure shows exposure time for two consecutive frames: 2× brightness.

High-Frame-Rate Video Capturing at Full HD

CMOS image sensors with Bright mode can capture videos at a rate of 240 fields per second at the interlaced Full HD video output. Furthermore, Toshiba will also provide an interlace-progressive conversion program that enables users to offer high quality progressive video with low deterioration, without changing frame rate.

This figure shows High-Frame-Rate Video Capturing at Full HD.

CMOS Image Sensors with Bright Mode

Part Number T4K82
Output Pixels 13M
Optical Format (inches) 1/3.07
Aspect Ratio 4:3
Pixel Pitch (µm) 1.12
Frame Rate (fps) Full Size/4K2K 30
1080p/720p 120 (Normal mode※1)
240 (Bright mode※2)
WVGA/VGA 240 (Normal mode※1)
480 (Bright mode※2)

  • ※1 Progressive output
  • ※2 Interlaced output. Frame rates are the values after progressive conversion processing.
  • Contacts

    If you have any questions, click one of these links:

    Technical queries
    Questions about purchasing, sampling and IC reliability
    ·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.