Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Parametric Search

Stock Check & Purchase

Select Product Categories

Image Recognition Processors Visconti™: Features

Feature 1: Parallel execution of up to eight image recognition applications

This is an example of simultaneous, parallel execution of multiple applications.

The Media Processing Engine (MPE) is suitable for image recognition and other multimedia processing. It is a very long instruction word (VLIW) machine that can issue multiple instructions simultaneously. It consists of Toshiba's proprietary low-power 32-bit RISC core called a Media Embedded Processor (MeP) and a coprocessor suitable for multimedia processing called Image Recognition VLIW Coprocessor 2 with FPU (IVC2F). IVC2F can execute one or two SIMD (single instruction stream, multiple data stream) instructions, which perform one or two operations on multiple data in parallel. The IVC2F can efficiently perform double-precision floating-point operations. The Visconti Family can execute multiple applications simultaneously* because of its multi-core configuration containing multiple MPEs.

* See the product specifications for details.

Visconti4 Block Diagram

TMPV760 Block Diagram

Feature 2: Image processing solutions that combine high speed and low power consumption

Image processing solutions that combine high speed and low power consumption

The Visconti Family contain image processing accelerators that perform the image processing required frequently in each step of image recognition at very high speed with low power consumption. The Visconti Family contain an affine transformation accelerator, which corrects any distortion of a fish-eye or wide-angle lens and performs point-of-view transformation. In addition, the Visconti Family contain filter accelerators, which perform noise reduction, edge detection, color space conversion and other image processing. The Visconti Family also include a histogram accelerator that creates histograms, and a matching accelerator that performs disparity calculation for a stereo camera system and motion detection. Furthermore, the Visconti Family contain a HOG accelerator, which handles Histogram of Oriented Gradients (HOG) / Toshiba Co-occurrence Histograms of Oriented Gradients (CoHOG) features that are suitable for robust human recognition. These processors can detect both moving and stationary pedestrians in real time. The Visconti4 Series incorporates an Enhanced CoHOG accelerator that combines luminance-based CoHOG feature descriptors with color-based feature descriptors obtained using a newly developed technique. It delivers a significant improvement in nighttime image recognition.

Feature 3: Toshiba’s original pattern recognition using multiple types of color features (Visconti4)

Toshiba’s original pattern recognition using multiple types of color features (TMPV760 Series)

In addition to the Toshiba-original luminance-based CoHOG, the image recognition accelerator contained in the Visconti4 processes four kinds of feature quantities: color-based CoHOG, Co-occurrence Histograms of Pairs of Edge Orientations and Color Differences (CoHED), Co-occurrence Histograms of Color Differences (CoHD), and Color Histograms. This accelerator provides high recognition performance even at nighttime and at scenes with less luminance differences between objects and the background. The Visconti4 realizes nighttime pedestrian recognition as reliable as daytime pedestrian recognition available with conventional vision systems.

Feature 4: General obstacle detection using 3D reconstruction technology (Visconti4)

Detection of Road Obstacles Using 3D Reconstruction Technique

While the Visconti2 and Visconti3 Series support the detection of pedestrians, vehicles and other objects using motion detection and pattern recognition, the SfM accelerator of the Visconti4 Series also makes it possible to detect general stationary obstacles such as fallen objects, fallen rocks and landslides without pre-learned object models. The Structure from Motion (SfM) accelerator provides three-dimensional (3D) reconstruction, a process of estimating 3D structures (distance, height and width) from 2D image sequences using a monocular (i.e., single) camera. 

This is an explanatory diagram of the general obstacle detection using 3D reconstruction technology.
* MIPI is a registered trademark owned by the MIPI Alliance.
* Microsoft and Windows are either registered trademarks or trademarks of Microsoft Corporation in the United States and/or other countries.
* Red Hat and Enterprise Linux are registered trademarks of Red Hat, Inc. in the United States and other countries.
* HDMI is a trademark or registered trademark of HDMI Licensing, LLC in the United States and/or other countries.
* MediaLB and MOST are registered trademarks of Microchip Technology Inc. in the United States and other countries.
* Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
* All other company names, product names, and service names mentioned herein may be trademarks of their respective companies.

Contacts

Technical inquiry

Contact us

Contact us

Frequently Asked Questions

FAQs

Queries about purchasing, sampling and IC reliability

Stock Check & Purchase

keyword:

A new window will open