Contact us

A new window will open A new window will open

Toshiba Announces Two New ARM® Cortex®-M4F Based Microcontrollers For Use In Both Home And Industrial Appliances

28 January 2015

TMPM470FDFG and TMPM475FDFG enable dual control of two brushless DC motors

Toshiba Announces Two New ARM® Cortex®-M4F Based Microcontrollers For Use In Both Home And Industrial Appliances

Toshiba Electronics Europe has announced two new products to join their range of ARM® Cortex®-M4F based TX04 series microcontrollers. Both the TMPM470FDFG and TMPM475FDFG are capable of operating two brushless DC motors simultaneously.
 

The new microcontrollers aim to satisfy ever-increasing demand for more energy efficient motors and incorporate vectoring technology to ensure highly efficient motor control. The TMPM475FDFG further integrates a CAN (Controller Area Network) controller which is required for use in specialist factory automation systems. Both chips are ideal for a wide range of uses ranging from industrial applications to use in home appliances, such as washing machines, fridges and air-conditioning units.
 

The TMPM470FDFG and TMPM475FDFG are based upon the high-performance ARM® Cortex®-M4F and can operate at up to 120MHz. They incorporate two modules, each containing a programmable motor drive, 12-bit AD converter and vector engine, ensuring the efficient and simultaneous operation of two brushless DC motors from a single chip.
 

Housed in a compact 14mm x 14mm LQFP100 package both the TMPM470FDFG and TMPM475FDFG offer an operating voltage ranging from 4.5 to 5.5V.
 

*ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. 
 

News Links

             

  High Resolution Image (jpg)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.