Contact us

A new window will open. A new window will open.

White LEDs

TL1L4 series

Toshiba offers white LEDs for lighting applications fabricated using a GaN-on-Si process in which a thin layer of gallium nitride is grown on a silicon wafer. These white LEDs help reduce the power consumption and cost of lighting equipment.

White LED Lineup

New lens top white LED “TL1L4 series“ is released!

LETERAS™

img_whiteled_02E

Toshiba's GaN-on-Si LED Chip Foundry

Toshiba's GaN-on-Si LED chips are manufactured by Kaga Toshiba Electronics Corporation.

img_led_02_1

img_led_03

Skipping Migration to 8-Inch Wafers

Toshiba's white LEDs are fabricated using 200-mm (8-inch) silicon wafers.

img_led_04

Application Examples

White LED are expected to find widespread use in more and more applications.

LED Bulbs, Residential Streets and Parks, Roads, LED Bulbs for Halogen Bulb Replacement, LED Base Lights...

LETERAS™ is the trademark of TOSHIBA CORPORATION.

Contacts

If you have any queries, click one of these links:

Technical queries
Queries about purchasing, sampling and IC reliability
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.