型號查詢

交叉搜尋

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

關鍵字搜尋

參數搜尋

線上庫存查詢跟購買

Select Product Categories

Features of the Toshiba Motor Control MCUs The Toshiba coprocessor enables easy and cost-effective vector control

Fields Oriented Control (FOC) is effective, but complicated and hard to use.

Inverter control of home appliances such as air conditioners has helped reduce their power consumption and enhance user experience. There are several methods of inverter control. The most commonly used method today is FOC that allows you to improve motor efficiency and reduce acoustic noise and vibration.
However, vector control involves complicated computation. For high-speed operation, it requires a combination of an expensive 32-bit MCU and an AD converter and thus entails difficult software development. Toshiba motor control MCUs simplify and reduce the cost of development of FOC applications.

Innovative Vector Engine that provides FOC

Toshiba has developed a coprocessor called the Vector Engine that quickly performs complicated computations of FOC. The Vector Engine eliminates the need for a part of software development. Toshiba motor control MCUs integrate the Vector Engine, a CPU and an AD converter on a single chip to simplify the use of FOC. Furthermore, the CPU is offloaded by passing FOC routines to the Vector Engine. Consequently, the CPU can operate at low speeds, reducing power consumption and cost. Instead of being depleted by FOC processing, the CPU resources are now available for sensor management and power supply monitoring so as to improve efficiency. Additionally, Toshiba motor control MCUs incorporate a suite of peripheral circuit blocks on the same chip to improve space utilization and motor control safety.

Benefits of the Vector Engine The VE reduces the CPU workload by 73%.

Industry-leading solutions using expertise accumulated over decades

Toshiba was the first company to offer MCUs with inverter control support. Since then, Toshiba has continuously endeavored to reduce the power consumption and improve the performance of motor applications. In the 1990s when a 16-bit MCU was primarily used for inverter control, Toshiba successfully realized inverter control by means of an 8-bit MCU with a programmable motor driver (PMD), reducing power consumption and cost. Toshiba subsequently released many MCUs incorporating a CPU and dedicated hardware, while, at the same time, accumulating expertise and offering industry-leading solutions for inverter control.

Commitment to enhancing ease of use

Since 2009, Toshiba has adopted ARM® cores. At present, Toshiba offers the M370 Group of MCUs with a ARM Cortext®-M3 core. Because ARM cores have a global user base, software can be reused across a wide range of applications and an extensive suite of tools are commercially available.
Toshiba also provides a development support environment that makes for a steep learning curve for novice FOC designers.
Toshiba is planning to further increase the speed of the MCU and the performance of the Vector Engine. Also on the agenda is incorporation a unique control technology in cooperation with the Corporate Manufacturing Engineering Center, which is involved in the R&D of electrical motors.

Features of the TMPM370 Group CPU resources are fully available for sensor processing and power supply monitoring. Reduces external part count and board size Improves motor control safety
* ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. All rights reserved.
A new window will open