April 26, 2010
TMPM380 Microcontroller Features 40 MHz CortexT-M3 Processor Core to Enable Increased Functionality and More Precise Operation
SAN JOSE , Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced availability of a new 32-bit microcontroller (MCU), the TMPM380. The TMPM380 MCU was specifically designed for the digital control of high-current circuits commonly found in industrial or appliance applications. Powered by a 40 MHz ARM® CortexT-M3 processor core, Toshiba's TMPM380 provides higher performance than the 8- and 16-bit MCUs typically used in industrial or appliance applications, yet at price points similar to the lower-performing alternatives. The new TMPM380 delivers improved operating characteristics, including better energy efficiency and more precise control.
The higher performance provided by the TMPM380 MCU also can enable the addition of new features to an application. For example, speech synthesis could be added to an appliance's user interface so the appliance could provide voice confirmation of user commands and settings. The TMPM380 MCU offers a 5V operation, which delivers better immunity to system noise than a comparable 3V MCU and easier interfacing with other 5V components.
"With the TMPM380 MCU, we are bringing a higher level of digital processing to industrial and appliance applications at a lower price point," said Andrew Burt, vice president of the Imaging and Communications Marketing Group in the ASSP Business unit at TAEC. "By implementing the TMPM380 MCU in their designs, engineers will be able to develop cookers, pumps, compressors, motors or any system controlled by inverters or discrete power devices with better operating characteristics or additional features without increasing system cost."
Toshiba's TMPM380 MCU uses a specialized pulse-width modulation (PWM) circuit, which can generate three-phase control for motor circuits or a 16-bit programmable pulse generator (PPG) control for circuits employing power semiconductors such as IGBTs ( insulated gate bipolar transistors) or FETs (field-effect transistors). The MCU has an on-board 12-bit analog/digital converter that can synchronize with the PWM unit to read back system state at critical times. The device also has several safety and fault tolerance features, including software support of the IED 60730B safety standard and oscillator frequency and low voltage detectors. An added benefit of the TMPM380 is that it uses zero-wait state FLASH and SRAM that assures latency time does not vary in unpredictable ways. As a result, designers can develop applications that require deterministic timing. This ability is key in applications requiring analog processing, where precise control loop timing is critical. In addition, the MCU's Cortex-M3 core offers fast interrupt response, especially important in applications where real-time operating systems need to quickly adapt to varying inputs, such as with appliances.
Engineering samples of the TMPM380 MCU are available now. Mass production is scheduled to begin in Q3 2010. The TMPM380 family pricing starts with the TMPM382FSFG (64K Flash / 8K SRAM) at $1.90 per unit in 10,000 unit quantities.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, distributions and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, discrete devices, displays, advanced materials, medical tubes, custom SoCs/ASICs, digital multimedia and imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, Preliminary 2009 WW Semiconductor Revenue Ranking, January 2010). For additional company and product information, please visit http://www.toshiba.com/taec/.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba’s "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook." This information is available at www.chips.toshiba.com or from your TAEC representative.
ARM is a registered trademark of ARM Limited. Cortex is a trademark of ARM Limited. All other brands or product names are the property of their respective holders. "ARM" is used to represent ARM Holdings plc; its operating company ARM Limited' and the regional subsidiaries ARM Inc.; ARM KK; ARM Korea Limited.; ARM Taiwan Limited; ARM France SAS; ARM Consulting (Shanghai) CO. Ltd.; ARM Belgium N.V.; ARM Germany GmbH; ARM Embedded Technologies Pvt. Ltd.; ARM Norway, ASA andARM Sweden AB
MCUS 10 591