New Toshiba Full HD CMOS Image Sensor Delivers High-Resolution Imagery To Security/Surveillance And Automotive Markets

March 18, 2013

Full HD (1080p) CMOS Image Sensor Offers Industry-Leading Dynamic Range and Fast Frame Rates for Optimum Viewing in High-Contrast Light Conditions

Toshiba TCM5117PL

SAN JOSE, Calif., – Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announces its newest device for the security/surveillance and automotive markets, a full HD (1080p) CMOS image sensor with industry-leading 100dB high dynamic range (HDR), fast frame rate of 60 frames per second (fps). The TCM5117PL is a CIS-type 1/3 inch optical format image sensor providing high-resolution picture quality in low-to-bright light conditions making it ideal for implementation in security/surveillance cameras and automotive systems.

"In the security/surveillance markets conventional CCD-based analog systems are rapidly being switched over to CMOS-based systems which better support security and the development of the network infrastructure," says Andrew Burt, vice president of the Analog and Imaging Business Unit, System LSI Group at TAEC." As such, we expect demand for these types of high-resolution CMOS image sensors to double in the next couple of years for both security/surveillance and automotive applications."

Toshiba's single-frame, alternate-row, dual-exposure HDR implementation in the TCM5117PL is well suited for capturing fast-moving objects compared to conventional multi-frame systems. With frame rates at 30 fps for conventional multi-frame systems, the single-frame approach, at 60 fps, promotes faster, less blurry and higher-quality images especially in high-contrast light conditions. The 2.7 um pixel size of the TCM5117PL is highly sensitive, and therefore offers better visibility and color-rich images in low-luminescent environments. In addition, the TCM5117PL is designed for long-term use, operating 24 hours a day.

The TCM5117PL has a 3.3±0.3V single-power supply and comes in a 10.5 x10.0 mm P-FLGA80 package. The device supports RAW10/RAW12 data formats.

Pricing and Availability

Samples of the TCM5117PL full HD CMOS image sensor are available Q2/2013. Mass production is scheduled for Q3/2013. Sample pricing is set at $35 (U.S.).

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's fifth largest semiconductor manufacturer (Gartner, 2012 WW Semiconductor Preliminary Revenue Ranking, December, 2012). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba's "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook"; This information is available at http://www.toshiba.com/taec/support/techquestions/index.jsp or from your TAEC representative.

ASSP 13 668

A new window will open