Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Power Management IC Optimizes Electronic Power Functionality For Consumer And Industrial Mobile Products

December 16, 2014

TC7734FTG

SAN JOSE, Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced a new system power management IC (PMIC) designed to help optimize power management functions for a wide range of mobile products. The TC7734FTG PMIC adopts a 130-nanometer analog semiconductor process with very low on-resistance and gate charge characteristics, and integrates various power management blocks within a single device

Rising demand for mobile products is driving concurrent growth in the market for PMICs, as manufacturers continually seek to reduce their products' power consumption. According to Transparency Market Research, the current compound annual growth rate for the global  PMIC market  (2013-2019) is currently 6.15 percent. By these statistics, the market will reach $46 billion by 2019.1

"Our customers often face conflicting challenges in battery-powered products where compact, efficient, and highly reliable power management solutions are needed in a short time-to-market window," said Deepak Mithani, senior director, Mixed-Signal Business Unit, System LSI Group at TAEC. "Toshiba is committed to providing power-management solutions that will help them to achieve these goals."

Power management blocks integrated by the TC7734FTG include power paths, switching charger, four-channel buck converters, three-channel low-dropout (LDO) regulators and two-channel LED backlight drivers. The charger block detects various USB™ port conditions and restricts the input current to 500mA, 1000mA or 1500mA, and all charger functions operate automatically without the need for any external control signals and it automatically changes the voltage source between the battery and USB connection as needed.

The IC also features an external thermistor that detects the battery's temperature, helping to prevent overheating while the mobile device is charging. Various thresholds and settings of the charger functions can be programmed by the onboard I2C interface. Individual settings of various output voltage levels, power sequences and many other functions can be programmed via I2C, with user-programmable eFuse to fit various platforms needs.

The TC7734FTG is housed in a compact 7mmx7mm QFN64 package with input voltage ranging from 3.4V to 5.5V. The IC integrates various error detect function, including thermal detect, over current limitation and LED open/short detection, to help ensure proper operation of smartphones, tablets, handheld medical devices, industrial PDAs, barcode readers and portable instruments.

Availability

Samples of the TC7734FTG PMIC are available now, with volume manufacturing set to begin in April 2015.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

1"Power Management IC Market - Global Industry Analysis, Market Size, Share, Growth, Trends and Forecast, 2013 - 2019," Transparency Market Research, Sept. 2014.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice.

USB is a trademark of Universal Serial Bus Implementers Forum, Inc.


POWR 14 735

A new window will open