Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba 13-Megapixel CMOS Image Sensor Addresses Area And Power Requirements For Mobile Devices

March 11, 2015

Chip is one of world's smallest, lowest-power-consumption 13MP sensors

13MP CMOS Image Sensors

SAN JOSE, Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced its newest 13-megapixel (MP) back-side illuminated (BSI) CMOS image sensor targeting smartphones and tablets. The T4KB3 is the world's smallest 13MP sensor1, and it reduces power consumption to 53 percent that of Toshiba's current 13MP sensor2, achieving 200 milliwatt (mW) output or less at 30 frames per second (fps).

Toshiba achieved these significant improvements over the previous-generation device by using a new design methodology to engineer the T4KB3. This approach was developed to meet mobile product makers’ continually increasing demand on chipmakers to produce CMOS sensors that can accommodate smaller form factors in tablets and smartphones. The new sensor also deploys Bright Mode technology, which helps prevent underexposed images in high-speed video recording by boosting image brightness up to 4x while realizing full-HD (1080p) video capture at 120fps equivalent.

"Toshiba listened to, and worked closely with, customers to develop this latest breakthrough in CMOS image sensor design," said Andrew Burt, vice president of the Image Sensor Business Unit, System LSI Group at TAEC. "Our new T4KB3 sensor was created to allow development of smaller, thinner camera modules that operate at low power while delivering the highest quality capture and playback of both still and video images - all capabilities that consumers want and will appreciate."

The T4KB3 has an optical size of 1/3.07 inch, 1.12-micron BSI pixel pitch, and 8Kbit one-time-programmable memory. The sensor can store lens shading correction data for two different conditions (e.g., indoors and outdoors), which have different light profiles. These conditions can be separately applied to image correction, and users can switch from one to the other with a simple command to achieve the best possible image capture.

Other products in Toshiba’s family of 1.12-micron BSI CMOS image sensors include the 8MP T4KA3, introduced in August 2014, and the 20MP T4KA7, launched in September 2014.

Availability

Samples of the T4KB3 CMOS image sensor are available now. Mass production is scheduled to begin next month.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

1 Toshiba research, as of March 2, 2015.
2 Compared with T4K82, introduced February 2014.

 

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
 

A new window will open