Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Automotive CMOS Image Sensor Features Industry-First LED Flicker Mitigation at 2 Megapixels

October 14, 2015

New sensor delivers high speed, accuracy; supports key automotive safety specs

Toshiba CSA02M00PB

SAN JOSE, Calif., – Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, has unveiled its newest CMOS image sensor for automotive cameras. The CSA02M00PB is the industry’s first1 2-megapixel (MP) CMOS image sensor to be equipped with LED flicker (pulsed LED) mitigation circuit2 to minimize image flicker caused by LED light sources. When recording LED traffic lights and signs with conventional CMOS image sensors, the output image often flickers, hindering sensing accuracy. Toshiba designed the CSA02M00PB to curtail this flickering and deliver clearer images for faster, more accurate image sensing.

The new sensor integrates Toshiba’s next-generation High Dynamic Range (HDR)3 system and backside illumination (BSI) process, which together enable recording of high-precision images. The HDR system uses Toshiba’s single-frame method to achieve clear images free of the degraded resolution and blown-out highlights typical of high contrast-light conditions. The BSI process, first1 brought to 2MP automotive image sensors by Toshiba, makes it possible to shoot brighter pictures with higher image quality in low light conditions.

Also of key value is the sensor’s ability to meet the requirements of Automotive Safety Integrity Level (ASIL), a risk classification scheme defined by ISO 26262 (the Functional Safety for Road Vehicles standard intended to protect life), and support failure detection, report flagging and control of vehicles. It is also compliant with AEC-Q1004 (Grade 2) and is suited for both ADAS front-end sensing cameras and the latest viewing applications, such as e-Mirror5 applications and camera monitor systems.

“With concerns for road safety continuing to escalate, ADAS technology is growing rapidly, and will be further spurred by future advances in driverless cars,” said Andrew Burt, vice president of the Image Sensor Business Unit, System LSI Group at TAEC. “Based on our internal estimates, Toshiba foresees three-fold growth in the automotive CMOS image sensor market by 2020. We look forward to collaborating with leaders in the automotive industry to continue developing CMOS image sensor business to fully meet the expanding requirements of this market.”

The CSA02M00PB features 3-micrometer BSI pixel size and an optical size of 1/2.7 inch. Image output ranges from 45 to 60 frames per second (fps), depending on the HDR exposure condition. Housed in 9x9 mm PBGA package, the sensor features full-HD output resolution of 1928(H) x 1084(V) and dynamic range of 120dB (by Toshiba calculation) with HDR. The MIPI CSI-2 serial interface facilitates the sensor’s integration into end products.

Availability

Samples of the CSA02M00PB CMOS image sensor will begin shipping in March 2016.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide.  A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor manufacturer and the world’s sixth largest semiconductor manufacturer (Gartner, 2014 Worldwide Semiconductor Revenue Estimates, December 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

Note: For further insights on the image sensor market, please follow the TAEC blog “Eye on Sensors.”
1Industry’s first as 2MP CMOS image sensor with LED flicker mitigation circuit. (Per Toshiba survey as of October 1, 2015.)
2A patented circuit designed to reduce the LED flicker defined in Europe’s EN12966 (LED light driven at a frequency of f>90Hz).
3Toshiba’s third-generation HDR that delivers a wider dynamic range than its predecessor, eliminating or suppressing resolution degradation and false color by enabling multiple exposures in one line of the image frame.
4AEC-Q100 refers to the stress test qualification for ICs established by the U.S.-based Automotive Electronics Council, which sets qualification standards for all electronics components supplied to the automotive industry.
5Mirror function that uses electronic components such as image sensors instead of conventional mirrors.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
 

A new window will open