Toshiba Extends Potential Applications for Wireless Power Charging with 15W Transmitter IC

February 23, 2016

Small, efficient Qi-compliant device enables mobile and industrial wireless charging

Toshiba TC7718FTG

SAN JOSE, Calif., – Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today launched a compact and efficient wireless power transmitter IC with a power transmission capability of 15 watts (W). Combined with a host microcontroller, the TC7718FTG realizes a wireless power transmission system compliant with Qi™ v1.2, the wireless charging standard. A 15W wireless transmitter system based on the new IC will allow quick recharging of devices – at a rate comparable to that of wired chargers.


Built on Toshiba’s proprietary, cutting-edge CD-0.13 semiconductor process[1], the TC7718FTG combines a compact package with high efficiency. This simplifies system integration and enables creation of charging systems with small footprints that are well suited for smartphone and tablet charging applications. In addition, the 15W rating of the device extends the possibility of wireless charging to industrial products and other higher power applications that may require more energy or shorter charging times than consumer devices.

“Consumer demand for wireless charging capability is rapidly evolving from ‘nice to have’ to ‘must have’,” said Deepak Mithani, senior director of the Mixed Signal Business Unit, System LSI Group at TAEC. “Toshiba foresaw this rise in demand, developing an offering of wireless receiver and transmitter ICs that are already being designed into commercially available charging stations. Now, with our 15W-capable products, developers will be able to meet the wireless charging demands associated with the most power-hungry mobile devices.”

Wireless transmitters that use the TC7718FTG will allow designers to create Qi v1.2 compatible charging stations capable of operating with powers up to 15W. This includes systems based on Toshiba’s recently announced TC7766WBG 15W receiver IC, which will be in mass production this spring, as well as the company’s TC7765WBG 10W receiver IC and TC7764WBG[2] 5W receiver IC, both of which are already in mass production.

Toshiba’s new electromagnetic induction transmitter IC integrates a full-bridge gate driver, a low-dropout (LDO) regulator with a 3.3V output and a low-pass filter for recovery of an amplitude shift keyed (ASK) signal[3]. The TC7718FTG is housed in a compact P-VQFN36 package and can handle input voltages from 4.5V to 25V. Operating frequency ranges from 110kHz to 205kHz. 

Availability

Sample shipments of the TC7718FTG wireless power transmitter IC are available now. Mass production is scheduled for spring 2016.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide.  A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 580 consolidated companies employing over 199,000 people worldwide. Visit Toshiba's web site at http://toshiba.semicon-storage.com.

1Based on 0.13-micron CMOS/DMOS semiconductor technology
2Compliant with Qi v1.1.2
3Qi-compliant wireless devices use ASK modulation to communicate between power receiver and power transmitter
Qi is a trademark of the Wireless Power Consortium.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications..
 

A new window will open