Contact us

A new window will open A new window will open

Company Milestones

Numerous Contributions to Technology and Society

logo_tosh_anniv

With nearly 130 years of operation, Toshiba has recorded numerous firsts and has made many valuable contributions to technology and society.

  • 2015

    • Toshiba introduces the industry’s first single-chip wireless power receiver that can operate at 15 watts and is compliant with Qi v1.2, wireless charging standard. (11/2015)
    • Toshiba delivers latest technology CMOS image sensors with NIR iris recognition for a more secure solution without the risk associated with lost or misused passwords. (10/2015)
    • Toshiba develops world’s first 256Gb, 48-Layer BiCS FLASH. (8/2015)
    • Toshiba develops world's first 16-die Stacked NAND Flash memory with TSV technology. (8/2015)
    • New Toshiba power receiver IC delivers quick charging of mobile devices, equivalent to that of charging your device via a cable. (8/2015)
    • Toshiba develops world's first 48-layer BiCS (Three Dimensional Stacked Structure Flash Memory). 3/2015
    • Toshiba has achieved an areal density of one terabit per square inch (1Tbit/ in2) within a 2.5-inch client hard disk drive (HDD). This newest disk drive innovation delivers 3TB capacity using a 750GB1 per platter in a 15mm 2.5-inch HDD and increases areal density over Toshiba’s prior generation of client HDDs by 40 percent. (2/2015)

  • 2014

    • Toshiba adds 6TB SATA and SAS models to its MG04 series of 3.5-inch form factor enterprise capacity class of hard disk drives (HDD). The new MG04 series 6TB models offer a 50 percent increase in max capacity from prior MG03 generation 4TB models and approximately 30 percent increase in sustained data rate. (2014)
    • Toshiba TLP385 transistor output photocoupler, in a low-height SO6L 4 pin package, with its low-height of 2.3mm (max) is 45 percent lower than DIP4 packages and can be used in applications with strict height requirements. (11/2014)
    • Industry's first Embedded DisplayPort™ (eDP™)-to-MIPI® dual-Display Serial Interface (DSI) converter chipset enables the 4K2K ultra high definition (UHD) experience for handheld electronic devices. (11/2014)
    • Toshiba class of e-MMC™ embedded NAND flash memory products are among the world's smallest integrating NAND chips fabricated with Toshiba's cutting-edge 15nm process technology and a controller to manage basic control functions into a single package. (10/2014)
    • Toshiba ships industry’s first samples of 32-gigabyte and 64-gigabyte (GB) embedded NAND flash memory modules compliant with the JEDEC UFS Ver.2.0 standard. (4/2014)
    • Toshiba developed the world's first 15-nanometer (nm) process technology, which will apply to 2-bit-per-cell 128-gigabit (16 gigabytes) NAND flash memories. (4/2014)
    • Toshiba released the industry’s largest-class storage capacity up to 600GB in a 15,000 rpm 2.5-inch HDD design.  (3/2014)

  • 2013

    • Toshiba ships 26 million Automotive-Grade HDDs.
    • Toshiba announces world's smallest 64-gigabit NAND memory chip on second generation 19 nanometer (nm) process technology.
    • Toshiba ships samples of industry's first universal Flash storage devices.
    • Toshiba starts second phase construction of No. 5 semiconductor fabrication facility at Yokkaichi.
    • Toshiba announces a 1/4 inch VGA CMOS image sensor for automotive sensor applications that combines a small chip-scale package (CSP) with through silicon via (TSV) technology for a 30 percent size reduction compared to other Toshiba products.
    • The TC358749XBG with HDMI to MIPI conversion enables HDMI video stream for the first time to be recognized and read directly by an application processor in a mobile device.
    • Toshiba ships largest capacity Automotive-Grade HDD in the World.
    • Toshiba ships 26 million Automotive-Grade HDDs.
    • The TMPM36BF10FG MCU offers the largest on-chip memory in its class with1MB flash ROM and 258KB SRAM including 2KB of backup memory.
    • Toshiba adds FFSA™ to its custom SOC product line. The metal configurable standard cell architecture enables rapid and cost effect implementation of ASIC/ASSPs and conversion of FPGAs in just weeks. Key benefits are 5X lower NRE than standard cell ASICS; 5X faster than FPGAs, 5X lower unit cost than FPGAs and 8 to 16X less power than FPGAs. Measurements are based on Toshiba benchmarks.
    • Toshiba has leveraged its new advanced process to create the T4K71 1080p Full-HD resolution CMOS image sensor with a smaller 1.12 micrometer pixel that has the same performance as a 1.4 micrometer pixel part.
    • Toshiba integrate s its superior Visconti™ image recognition processor with an ARM® Cortex™-A9 MPCore™, two A9 CPUs and an FPU for improved performance, connectivity and better system integration.

  • 2012

    • Toshiba begins volume production of Solid State Hybrid Drives - combining the performance of Flash with the capacity of HDD.
    • Toshiba ships first cSSD drives based on 19nm process NAND Flash technology.
    • T oshiba marks 25th anniversary of invention of NAND Flash technology.
    • Toshiba expands high-performance memory card family with first microSDHC™ UHS-I EXCERIA products.
    • Toshiba announces next-generation Superjunction technology for power MOSFETs.
    • Toshiba launches SDHC memory cards with world's fastest transfer rates.
    • Toshiba announces first LSI featuring TransferJet™-breakthrough technology for wireless transfer/streaming of large files just by touching two devices together.
    • Toshiba develops, manufactures 19nm generation NAND Flash Memory with world's largest density and smallest die size - 128 Gb capacity in a 3-bit-per-cell chip on a 170mm2 die.

  • 2011

    • Toshiba and SanDisk celebrate the opening of Fab 5 300mm NAND Flash Memory fabrication facility in Japan.
    • Toshiba launches 19nm process NAND flash memory. The world's finest process yields single chips with a 64 gigabit capacity.
    • Toshiba introduces SmartNAND™ a new 24nm embedded-NAND flash memory with integrated Error Correction Code and NAND interface to simplify product development.

  • 2010

    • Toshiba introduces Enterprise SSDs with 32nm eSLC NAND flash.
    • Toshiba announced the launch of 8GB (gigabyte) 16GB1 and 32GB SDHC UHS-I cards compliant with the SD Memory Card Standard Ver. 3.0 (SD 3.0), UHS104. These new SD cards offer the world's fastest2 SDHC data read and write speeds.
    • Reinforcing its leadership in the development and fabrication of cutting-edge, high density NAND flash memories, Toshiba announced that it started mass production of NAND flash memories fabricated with 24nm3 process technology. This latest technology advance has already been applied to 2bit-per-cell 64-gigabit (Gb)4 chips that are the world's smallest and offer the highest density on a single chip (8 gigabytes (GB))4.
    • Toshiba launched a 128-gigabyte (GB) embedded NAND flash memory module, the highest capacity yet achieved in the industry5.

     

    1Product density is identified based on the maximum density of memory chip(s) within the Product, not the amount of memory capacity available for data storage by the end user. Consumer-usable capacity will be less due to overhead data areas, formatting, bad blocks, and other constraints, and may also vary based on the host device and application.
    2As of September 2, 2010.
    3nm = nanometer (1 billionth of a meter).
    4Source: Toshiba Corporation, August 2010.
    5For embedded NAND flash memory modules. Source: Toshiba, June 2010.

  • 2009

    • Toshiba acquires Fujitsu HDD business, creating the broadest portfolio of products in the storage industry
    • Adds complete system backup and password-protected encryption to personal storage line
    • Adds 500GB USB 2.0 portable external hard disk drive (HDD) to personal storage line
    • Toshiba continues to take leadership in the smallest possible process geometries producing custom chips in 65nm and 40nm and memory devices in 43nm and 32nm, with even more advanced processes in development.
    • Toshiba had 1,669 utility patents granted in the United States in 2009, ranking 5th in the world for total number of patents granted between 1969 and 2009 (U.S. Patent Office). Many of the breakthroughs we've pioneered have been critical to customer successes.
    • Toshiba is a leader in the energy business, and its ground-breaking efforts in Direct Methanol Fuel Cell (DMFC) technology have now culminated in the delivery of Toshiba's first commercial power source for market testing in Japan.
    • Toshiba has incorporated an LED backlight system with up to 100,000 hours MTBF1 at ordinary room temperatures (25°C) for industrial applications.  The innovative backlight system achieves increased longevity through design optimization for heat dissipation and luminous efficiency.
    • Toshiba develops the industry's highest capacity, 128GB e-MMC embedded NAND Flash module (announced 6/16/10).
    • Toshiba introduces industry's first 64GB SDXC memory card.
    • Toshiba Makes Major Advances in 3-bit-per cell and 4-bit per cell 32nm NAND Flash.
    • Toshiba Develops World's Highest Bandwidth, Highest Density Non-Volatile RAM, a 128Mb, 1.6GB/sec FeRAM.
    • Toshiba Matsushita Display Technology Previews Integration Of High Resolution 3D Capabilities Into Handheld Devices at CES.
    • Toshiba, and its technology partner SanDisk, announced the world's smallest 32nm 3-bit NAND flash chip at the February ISSCC 2009, with a die size of 113mm.

     

    1Based on MTBF statistical values. MTBF (Mean Time Between Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may not resemble the MTBF.

  • 2008

    • Brings SATA technology to automotive HDDs with 80GB model
    • Introduces 250GB 1.8-inch Micro SATA HDD for computing applications
    • Announces 240GB 1.8-inch PATA HDD for compact consumer electronic and computing applications
    • Launches highest capacity 2.5-inch HDD - 400GB
    • Commences production of reduced halogen and other potentially hazardous substances with its 160GB/platter 5400 RPM 2.5-inch series
    • Debuts series of third-generation high-performance 2.5-inch 7200 RPM HDDs
    • Ships slim 160GB 1.8-inch 5400 RPM Micro-SATA HDD
    • Brings highest capacity portable external hard drive to market with 320GB USB 2.0-enabled solution
    • Ships first 6Gb/s Serial Attached SCSI (SAS) enterprise HDDs*
    • First HDD manufacturer to meet the OPAL encryption specification*
    • Toshiba Launches 43nm SLC NAND Flash Memory
    • Toshiba Launches Its First ARM® Cortex-M3™ Microcontroller
    • Toshiba Launches Largest Density Embedded NAND Flash Memory Devices
    • Toshiba Starts Sample Shipping Of SpursEngine™ SE1000 High-Performance Stream Processor
    • Toshiba, Sony Corporation and Sony Computer Entertainment Inc. Announce an Agreement to Form a New Joint Venture for the Production of High-performance Semiconductors, including Products for SCEI's PlayStation Computer Entertainment Systems
    • Toshiba Launches First 32-Bit Microcontroller With ARM926EJ-S Processor
    • Toshiba Adds High Efficiency, 35A DrMOS-Compatible Multi-Chip Module For DC-DC Converters In Servers
    • Toshiba and SanDisk announce sampling of 16Gb 43nm MLC NAND
    • New Industrial LCD Panels With Long-Life LED Backlighting Systems From Toshiba America Electronic Components, Inc.
    • Toshiba Expands GaN HEMT Product Family With Power Amplifiers For Ku-Band Satcom And X-Band Radar Applications
    • Development of Small-Molecule Organic EL Display Panels Achieves Lifetime of 60K1 Hours and the World's Highest-Level Performance
    • Toshiba Matsushita Display Technology Co., Ltd. working in joint development with Idemitsu Kosan Co., Ltd. completes organic EL element featuring low power consumption and extended lifetime
    • Toshiba DTMOS II Family Of 600V Power MOSFETs Use Superjunction Structure To Increase Power Efficiency
    • First 512GB Multi-Level Cell Solid State Drives

  • 2007

    • Introduces the industry's first 300GB 2.5-inch external HDD*
    • Launches the first 15K 2.5-inch HDD with SAS interface*
    • Achieves highest areal density demonstration at one terabit per inch using patterned media*
    • Offers first 1.8-inch HDD with CE-ATA interface.
    • Enters personal storage market with a line of portable USB 2.0 external hard drives
    • Toshiba And IBM Extend Semiconductor Research And Development Collaboration for 32nm CMOS Process Technology
    • Toshiba Launches High Performance Solid State Drives With MLC NAND Flash Memory
    • Toshiba to Enhance Competitiveness In Image Sensor Business By Bringing Manufacturing Of CMOS Camera Modules For Mobile Phones In-House
    • Toshiba Launches New Line Of Ultra-Compact Camera Modules Featuring Image Sensor Technology
    • Toshiba and SanDisk Inaugurate New 300mm Wafer Fab 4 for NAND Flash Memory At Yokkaichi Operations
    • Toshiba Develops Wide Dynamic Range Technology For CMOS Image Sensors; Will Enable Camera Phones To Capture More Image Detail In Both Bright Light And Deep Shadows
    • Toshiba Achieves Mobile Strategic Initiative Milestone With Launch Of Enhanced MIPI™ Display Buffer/Controller, The World's First Display Controller To Support The High-Speed MIPI DSI Standard
    • Toshiba Ships 56nm NAND Flash Memory
    • Toshiba reveals strategic initiative for mobile handset market to speed time-to-market with flexible, modular analog peripheral and mixed-signal building blocks
    • Toshiba announces MIPI Display Controller that supports the high-speed MIPI DSI standard
    • Toshiba retains position as the number one ranked supplier of optoelectronics, sensor/actuators and discrete components (OSD) in 2007 (April 2007, IC Insights), for the 22nd year
    • TAEC and TMD announced an expanded line-up of RoHS-Compatible industrial LCD displays, including an ultra high-luminance 12.1-inch SVGA LCD for outdoor use
    • Toshiba introduces its first commercial GaN semiconductor, a 50W, X-band HEMT for radar and medical applications
    • New Toshiba 50MBd High Speed Photocoupler Is The Fastest Yet In The Company's Lineup
    • Toshiba Expands LED Product Line With Compact New Generation White LEDs That Are Twice As Bright
    • Toshiba and SanDisk mark the opening ceremony for a second 300 mm wafer fab at Toshiba's Yokkaichi Operations, due online in Q407 to meet fast growing demand for NAND flash memory
    • Toshiba Announces Gallium Nitride Power FET With World's Highest Output Power In Ku-band
    • Toshiba introduces a family of MLC NAND based solid state disk drives

  • 2006

    • Leads market with 200GB 2.5-inch 5400 RPM HDD
    • Extends perpendicular magnetic recording (PMR) reach to 0.85-inch and 2.5-inch HDD offerings
    • Hitachi, Toshiba and Renesas Agree to Establish Semiconductor Foundry Planning Company
    • Toshiba Announces 16-Gigabit Multi-Level Cell Nand Flash Components Using 70-Nanometer Process Technology
    • Toshiba Showcase 6GHz, 174W Gallium Nitride Power FET At MTT-S; Unveils Roadmap For GaN Microwave Devices
    • Toshiba Expands Frequency Ranges Of 9W And 30W Extended Ku-Band GaAs FET Lines For VSAT Satellite Communications
    • Toshiba America Electronic Components Announces Expanded Line-Up RoHS-Compatible Industrial LCD Displays, Including An Ultra High Luminance 12.1-Inch SVGA LCD For Outdoor Use
    • Toshiba rolls out second-generation, single-chip solution for mid-range and low-end digital TV applications driven by the Congressional mandate that all U.S. broadcast televisions must be completely converted to digital terrestrial transmissions by 2009
    • Toshiba, Sony Corporation and NEC Electronics Corporation announce the successful co-development of an LSI mass production platform for next-generation 45 nm process technology

  • 2005

    • Expands engineering expertise with acquisition of Matsushita's U.S.-based HDD Design Division
    • Ships 100 millionth HDD
    • First to commercialize PMR, achieving 133 gigabits per square inch on 1.8-inch HDD
    • Toshiba Announces Line-Up Of Toshiba-Branded USB 2.0 Flash Drives Plus Customizable USB 2.0 Flash Drive Subassemblies For OEMs

  • 2004

    • Recognized in the Guinness World Recordsâ„¢ for world's smallest HDD (0.85-inch)
    • Announced world's first 2.5-inch SAS Enterprise HDD*
    • Toshiba Announces Expansion Of Power Mosfet Packaging Solution With Smaller, Thinner TSSOP Advance Package With Lead-Free Finish
    • Toshiba Expands Family Of SOP Advance Mosfets With 8 New Lead-Free Finish Devices For Greater Power Efficiencey
    • Toshiba Announces Industry's Smallest GaAs MESFET Switch For Multi-Band/Multi-Mode Cellular, Bluetooth and WLAN Applications
    • Toshiba Announces World's Smallest Safety-Standard Compliant Photocoupler
    • Toshiba, Xilinx Announce Strategic Foundry Relationship, Reach 90nm/300mm Manufacturing Milestone
    • Toshiba Expands World's Smallest LMOS Logic IC Series With Low Voltage, Low Power Consumption Devices
    • Toshiba Announces Availability Of White Paper On Lead(Pb)-Free Manufacturing And Products International Electrotechnical Commission Forms Working Group To Set Industrial Standard For Micro Fuel Cells
    • Toshiba Unveils New Smart Thin Package For Power MOSFETs With Industry's Smallest Mount Area Per Milliohm Of On-Resistance
    • Toshiba Announces World's Smallest Direct Methanol Fuel Cell With Energy Output Of 100 Milliwatts
    • Toshiba To Start Production Of Industry's First SOC With The X Architecture
    • Toshiba Debuts First Full-Color "System On Glass" (SOG) Input Display With Image Capture Technology
    • Toshiba Introduces New 1.8v Multi-Chip Package Memory Solutions With Burst Mode Capabilities For Next-Generation Cellular Phone Applications
    • Toshiba Tapes Out Multiple 90-Nanometer SoC Designs With Synopsys' Galaxy Design Platform
    • Toshiba Starts the Construction of State-of-the Art Wafer Fab For NAND Flash Memory At Yokkaichi Operations
    • Toshiba Unveils 512Mb Network FCRAM™, The Industry's Largest Density Low Latency DRAM For Network Applications
    • Toshiba Takes NAND Flash Memory To 4-Gigabit Level Using 90 Nanometer Process Technology
    • Toshiba Completes Construction of Building for 300mm Wafer Fab at Oita Operations in Kyushu
    • Toshiba Matsushita Display Technology Announces World's Lowest Power 14.1-Inch Displays For Mobile PCs
    • Agere Systems First Company To Offer Multiple Sources Of Low-Latency, DRAM Memory Chips For Network Processor Customers
    • Toshiba Develops Multi-Chip Package (MCP) Which Realizes Stacking Of 9 Layers With 1.4MM Thickness.

  • 2003

    • Introduces the world's first 2.5-inch SATA HDD*
    • Toshiba Offers New Line Of 1200V IGBT Modules Using Injection Enhanced Gate Transistor Process Technology To Achieve Higher Performance
    • Toshiba Introduces New PS-8 Lead-Free Ultra-Thin Package For MOSFETS And Low Saturation Bi-Polar Transistors
    • Toshiba Introduces New Family of Power MOSFETs With Advanced Process Technology To Enable Faster Switching Speeds
    • Toshiba Discloses SoCMosaic™ Custom Chip Hardware/Software Co-Development Strategy And Announces First Two Supported Environments, SwordFish And Seamless
    • Toshiba Announces World's Smallest Direct Methanol Fuel Cell With Energy Output Of 1 Watt To Be Used For Portable Devices
    • Toshiba Announces MOSFETs Using New SOP Advance Packaging And Ultra High Speed Process Technology For Improved Power Efficiency
    • Toshiba Offers Lead-Free Versions Of All Its NAND Flash Memory Devices In TSOP Packages
    • Toshiba Licenses High-Performance ARM Core For Custom SoC Business
    • Toshiba America Electronic Components, Inc. Announces Plans To Implement Lead-Free Manufacturing Supporting Industry Environmental Initiative
    • Toshiba Adds Wider, x16 NAND Flash Memory For Faster Read Cycles In Cell Phones And Mobile Electronics Applications
    • Toshiba Offers Complete MCP Solutions For Cell Phones With NOR Flash, NAND Flash, SRAM, Pseudo SRAM Or Low Power SDRAM
    • Toshiba Announces 2-Gigabit NAND Featuring Automatic Erase And Program Operations For File Storage Applications
    • New Toshiba CMOS Image Sensor Camera Enables Wireless Transmission Of High-Quality Photos For Next-Generation Phones And PDAs
    • Toshiba And SanDisk Announce Novel NAND Cell Architecture Enabling Major Advances In Flash Memory Capacity
    • Toshiba Announces The Industry's First 90-Watt C-Band GaAs FET For Satellite Communications
    • Toshiba Expands 60-Watt C-Band GaAs FET Product Line To Provide New SSPA Market Opportunities For Satellite Communications
    • Toshiba Announces Highest Output Power Ku-Band GaAs FET For VSAT Satellite Communication Applications
    • Toshiba Announces Industry's First Single Die MOSFET And Schottky Barrier Diode For DC/DC Converters
    • Toshiba Launches Two New 64-Bit RISC Microprocessors, Its First Standard Processors Based On Leading-Edge 90nm Process Technology
    • Toshiba Announces Mosfets Using New Ultra High Speed Process And Revolutionary Bonding Technology For Improved Power Efficiency
    • Toshiba Extends High Luminosity White LED Offering With Addition Of Bluish Green And Purple LEDs
    • Toshiba America Electronic Components Demonstrates First "System On Glass" (SOG) Input Display With Built-In Image Capture
    • Toshiba Launches First SoCMosaic Custom Chip, An Arm-Based Controller For Low-End Networking And Consumer Convergence Applications
    • Toshiba Rolls Out New Single-Chip High-Definition Digital Multimedia Decoder Chip
    • Toshiba's White LED Selected As Recipient Of The 2002 Photonics Circle Of Excellence Award
    • Toshiba Develops Five- And Six-Chip Multi-Chip Packages Combining NOR Flash, SRAM, Pseudo SRAM And NAND Flash For Advanced Cell Phone Applications
    • Toshiba Adds Modified NAND Flash Memory For Easier Integration In Advanced Cell Phones With Complex Memory Subsystems
    • Toshiba Adds High-Speed Transmitter/Receiver For Automotive Lan To Its TOSLINK™ Family Of Fiber Optic Devices
    • M-Systems And Toshiba Unveil Mobile DiskOnChip G3 - The World's Smallest High-Capacity NAND-Based Memory Solution
    • Toshiba Announces 32-Megabit FeRAM Developed With Infineon
    • Toshiba Launches SoCMosaic Custom Chip Platform
    • Toshiba Announces 128Mb Pseudo SRAM Family; Highest Density Available For Mobile System Applications
    • Toshiba Tells Advanced Soc Strategy, Launches 90NM TC300 Family Targeted At High-Performance Applications.

  • 2002

    • Introduces U320 SCSI drive*
    • Toshiba And Sony Make Major Advances In Semiconductor Process Technologies
    • AFPD Pte. Ltd. Celebrates Official Plant Opening And Start Of Production Of Advanced TFT-LCDs In Singapore
    • Toshiba Expands Silicon Germanium Transistor Line Up With Industry's Smallest Package
    • Sandisk and Toshiba Announce Development of 90 Nanometer Process Technology for Binary and MLC NAND Flash
    • Toshiba America Electronic Components, Inc. Becomes First Semiconductor Company to Receive New C-TPAT Customs Certification
    • Toshiba Adds To High-Performance Memory Portfolio With 333MHz Network FCRAM™ Family For Networking And Server Applications
    • New Voltage Regulator IC for Automotive Applications from Toshiba Achieves World's Lowest Power Consumption
    • M-Systems and Toshiba Sign Collaboration Agreement Pertaining to Development, Marketing and Supply of New DiskOnChip Products
    • New CISC 32-Bit Microprocessor from Toshiba Combines Integrated Color LCD, USB and NAND Flash Memory Controllers and Attains World's Lowest Power Consumption
    • New RISC Companion Chip from Toshiba is First IC with On-Chip ATA/ATAPI, USB Device/Host, I2C and PCI Controllers
    • Toshiba Announces the Industry's Highest Power Ku-Band GaAs FET for Satellite Communications
    • Toshiba Reaffirms Commitment to LCD Market Through the Development of Advanced Display Solutions
    • Toshiba Announces the Industry's Lowest Power Consumption Photocoupler
    • Toshiba Announces the Industry's First 60 Watt Extended C-Band GaAs FET for Satellite Communications
    • IBM, Sony, SCE and Toshiba to Jointly Develop Chip-Making Process Technology
    • Toshiba Develops the World's Smallest Stacked Multi-Chip Package Currently Available
    • Electronic Products Magazine Chooses Toshiba's White LED As One of the 2001 "Products of the Year"
    • Agere Systems Selects Toshiba's FCRAM For Use With OC-192 PayloadPlus Network Processor
    • Artile, Simplex and Toshiba present first application of the X Architecture as ISSCC
    • Toshiba and Matsushita Announce Outline of New LCD Joint Venture
    • Toshiba Named EDN 2001 Innovation of the Year Awards Finalist for its MPEG-4 Video CODEC
    • Toshiba Enters U.S. Automotive Market With Cost-Effective Single Chip Solution For Car Information Systems.

  • 2001

    • Starts utilizing environmentally sound printed circuit board assemblies (PCBA) in all new HDD products
    • Commences volume production of first HDD designed for automotive applications
    • Toshiba's New Regulator IC Offers The World's Lowest Current Consumption For Automotive Applications
    • Toshiba Debuts One-Gigabit NAND Flash Memory Device
    • Toshiba and Matsushita to Establish a Joint Venture for Procurement of Parts and Materials for CRT Production
    • Toshiba and Matsushita to Unify LCD Business
    • Toshiba Introduces First NAND Flash Drives Optimized For Industrial Applications
    • Toshiba Announces Industry's First 64Mb Pseudo SRAM Family
    • TAEC Introduces EDRAM Core With 12-Ns Access Time For SRAM Replacement; New ASIC Capability Delivers Fastest Access Time In 0.18-µM CMOS
    • Toshiba Has First Microcontroller With SD Memory Card Controller
    • Toshiba Unveils Its Roadmap For Continued Leadership In The Flash Memory Market
    • Simplex And Toshiba Change The Face Of Chip Design By Enabling Revolutionary IC Architecture
    • Semiconductor Industry Leaders Launch Initiative To Support Radical New Chip Architecture
    • Toshiba Develops World's First 260,000-Color Polymer Organic Light Emitting Display
    • Toshiba Expands Industry-Leading Portfolio Of Microwave Components With New Modules For Telecommunications Infrastructure Equipment
    • Toshiba And Avnet Form Global Distribution Network
    • Toshiba Joins Forces With Arrow Electronics To Create Global Distribution Network
    • Toshiba America Electronics Components Launches ArTile Microsystems To Provide Rapid System-On-A-Chip Designs
    • Toshiba And Sony Computer Entertainment Inc. To Make A Technical Alliance For 0.13 Micron Rule Semiconductor Embedded DRAM Logic Process
    • Sony Computer Entertainment Inc., IBM And Toshiba Join To Develop "Supercomputer-On-A-Chip" For The Broadband Era
    • Toshiba Introduces Advanced Lithium Batteries For Sleeker, More Compact Designs In Wireless Communications Devices
    • Toshiba Announces Development Of White LED
    • Toshiba Announces The World's First Single-Channel Interface Driver ICs
    • Toshiba Launches World's First 32-bit CISC Microcomputers with Memory Integration.

  • 2000

    • Debuts the first high-volume 1.8-inch HDD, igniting the start of the digital music revolution
    • Breaks the areal density world record with 56 gigabits per square inch*
    • Toshiba's New Fabrication Method of Gate Oxide for MOS Devices Will Improve Long-term Reliability of LSI
    • EDN Magazine Names Toshiba's NAND Flash Memory One Of Its Hot 100 Products Of 2000
    • Toshiba Announces Availability Of World's First Low-Power, Single-Chip MPEG-4 Decoder.
    • Toshiba Launches First Portable PC Host-Controller LSI For SD Memory Card And SmartMedia
    • Toshiba And Tessera Announce Innovative Technology Licensing Agreement
    • Amkor And Toshiba Form Joint Venture; First Major Assembly And Test Foundry In Japan
    • Toshiba America Electronic Components, Inc. Introduces New Online Technical Support On Web Site
    • Toshiba Introduces World's First 8.4-Inch SVGA Low-Temperature Poly-Silicon TFT LCD For High-Brightness Industrial Applications
    • Toshiba Introduces World's First 5.8-Inch And 7.0-Inch High-Resolution, Wide-Format, Low-Temperature Poly-Silicon TFT LCDs
    • Toshiba Introduces The Industry's First Embedded 64-Bit MIPS CPU SLI ASIC Core
    • Toshiba To Build Advanced System IC Facility At Its Oita Plant
    • Toshiba Demonstrates World's First 4-Inch, 202 Pixel Per Inch Color Reflective Low Temperature Poly-Silicon TFT LCD
    • Toshiba Makes Major Investment In Facilities For Large-Sized Low-Temperature Poly-Silicon TFT LCDs
    • Toshiba Develops Industry's First 64Mb Read While Write Nor Flash Memory Device
    • Toshiba Details World's First Single-Chip MPEG-4 Videophone LSI With Embedded 16MBIT DRAM At ISSCC
    • Microprocessor Report Names The Sony/Toshiba Emotion Engine Best Embedded Processor Of The Year.

  • 1999

    • Introduces U160 SCSI drive*
    • Leads the areal density race by breaking the 20 gigabits per square inch barrier*
    • Toshiba and SanDisk agree to jointly develop and jointly manufacture gigabit scale flash memories
    • Toshiba develops world's first 15-inch Low-Temperature Poly-Silicon TFT LCD with UXGA resolution
    • Toshiba introduces the smallest and thinnest five-pin CMOS Logic package
    • Toshiba announces plan to buy out IBM's stake in Dominion Semiconductor joint manufacturing venture in Manassas, VA, by Dec. 2000, and use additional capacity for DRAM and NAND production
    • Toshiba introduces world's smallest, thinnest 16-pin and 20-pin CMOS Logic packages
    • Toshiba develops industry's first 512Mb NAND Flash components and 64MB SmartMedia cards by packaging two 256Mb NAND die in TSOP and SmartMedia packaging
    • Toshiba introduces the industry's first internally matched 60-Watt C-Band GaAs FET
    • Toshiba releases 0.14µm SLI ASIC Libraries with Embedded DRAM and application-specific cores
    • Toshiba's new Low-Temperature Poly-Silicon LCD facility begins operation in Fukaya, Japan. Fukaya Works is Toshiba's first facility dedicated to the production of large-size, Low-Temperature Poly-Silicon TFT LCD's
    • Toshiba launches industry's smallest 128Mb and 144Mb Rambus DRAM die
    • Toshiba moves up from the world's fifth largest semiconductor supplier to fourth in Dataquest rankings
    • Toshiba develops first prototype of a nonvolatile Chain Ferro-electro RAM (Chain FRAM). Breakthrough design combines high-speed read and write operations with a small chip size and surpasses the performance of existing FRAM
    • Fujitsu and Toshiba announce joint development agreement for Fast Cycle RAM (FCRAM) in 64-, 128- and 256-Megabit densities to achieve operation cycles two to three times faster than conventional DRAMs
    • Toshiba announces its 4-inch Low-Temperature Poly-Silicon TFT LCD technology
    • Toshiba enables 350mips/W performance with new TMPR1940 microprocessor family
    • Toshiba licenses ARM7TDMI RISC Core
    • NEC Corporation and Toshiba Corporation expand their commitment to MIPS Technologies, Inc.

  • 1998

    • First manufacturer to transition to GMR across its product line*
    • Introduces first HDD to utilize giant magneto resistive (GMR) recording head technology to achieve 2.16GB on one 2.5-inch disk
    • Toshiba produces world's first 0.25-micron embedded DRAM ASIC for Pixelworks' Image Processor
    • Toshiba and Fujitsu announce collaboration to develop next-generation 1-Gigabyte DRAM.
    • Toshiba announces the industry's first 8.4- and 10.4-inch Low-Temperature Poly-Silicon LCD's
    • Toshiba deploys global Scalable by Design™ program and manifests quick process migration for industry-leading manufacturing efficiency
    • Production of Color Display Tubes begins at Toshiba Display Devices, Horseheads, NY
    • Toshiba announces first microprocessor from TX49 Family; 64-bit processor boasts world's lowest 64-bit power consumption at 1.2 watts
    • Fujitsu, NEC and Toshiba agree on specifications for stacked Multi-Chip Packages compatible with all high density Flash memory and SRAM for cell phones and other handheld devices
    • Toshiba debuts new high-performance 8-Bit microcontroller series.
    • Toshiba introduces first shadow mask flat face Color Picture Tube in Japan
    • Toshiba begins qualified production of 64Mb DRAMs at Dominion Semiconductor, and Toshiba's 64Mb SDRAM secures Intel® PC100 validation
    • TAEC adds Disk Products Division to its operations; product offerings now include Hard Disk, CD-ROM and DVD drives
    • The Low Voltage Alliance introduces the 2.5V VCX family, the first industry standard product offering to provide mixed-voltage compatibility with both 3.6V and next-generation 1.8V components
    • Toshiba's 0.25-micron System-Level ASIC family integrates more than 10 million usable gates
    • Toshiba announces the industry's first reflective and low-temperature poly-Silicon (LTPS) TFT LCD technology

  • 1997

    • Toshiba introduces its MIPS RISC Development Platform for Window CE-based applications
    • Toshiba announces architecture for new low-power TX19 microprocessor family
    • Toshiba claims world leadership in Embedded DRAM with proprietary trench process
    • The Low Voltage Logic Alliance (Toshiba, Fairchild and Motorola) announces the industry's first 2.5V CMOS logic standard with 3.6V-tolerant inputs and outputs
    • Toshiba licenses MIPS16™ Architecture; announces roadmap for full line of MIPS RISC microprocessors from 32-bit through 64-bit

  • 1996

    • Toshiba develops world's first circuit technology for 0.5V operation of ICs
    • Toshiba and Samsung Electronics to cooperate on Solid State Floppy Disk Card SmartMedia storage solution
    • Toshiba enters the Surface Mount LED market
    • Toshiba develops first self-pulsating Laser Diode for DVD applications
    • Toshiba first with Press Pack IGBTs

  • 1995

    • Toshiba develops innovative capacitor structure for 1-Gigabit DRAM memory cell. The highly compact bottle-shaped trench capacity enables development of smaller, more efficient DRAM cells
    • Toshiba and Winbond enter partnership to produce and develop semiconductor memory devices
    • Toshiba develops unique data storage medium for small form factor applications: Solid State Floppy Disk Card
    • Motorola to join alliance of IBM, Siemens and Toshiba to develop advanced memory devices
    • Toshiba announces partnership with Digital Equipment Corporation to jointly develop highly optimized 155 ATM SAR LSI's
    • Toshiba and IBM form Dominion LLC joint venture to produce DRAM in Manassas, VA
    • IBM, Siemens and Toshiba alliance announces smallest fully functional 256Mb DRAM
    • Toshiba strikes alliance with Samsung for joint development of 64Mb NAND Flash memories
    • The Low-Voltage Logic Alliance introduces LCX as its first, high-performance, low-voltage product, with over-voltage tolerance. This standard is also supported by SGS-Thompson and Pericom
    • Toshiba introduces microfilter™ for Color Display Tubes. Toshiba introduces its multimode Communications Laser Diodes (CLDs)
    • Toshiba unveils its R3900 32-bit microprocessor core

  • 1994

    • Toshiba completes ISO 9001 requirements
    • Vertex Semiconductor merges into Toshiba America Electronic Components and becomes part of the System IC group
    • Toshiba granted Pre-Importation Review Program (PIRP) status by U.S. Customs in recognition of superior trade compliance performance
    • Display Technology, Inc. announces increased capacity for the manufacturing of TFT LCDs

  • 1993

    • Toshiba and Synopsys announce cooperation in high-level design automation for next-generation ASICs
    • Toshiba introduces its 16-bit microcontroller family
    • Toshiba receives ISO 9000 certification
    • Toshiba joins with National Semiconductor and Motorola Semiconductor Products Sector to form the Low-Voltage Logic Alliance to develop standards and common specifications for logic and jointly introduce and promote high-performance, low-voltage CMOS logic products
    • Toshiba first to offer 1700V IGBTs
    • Toshiba offers its R4600 32-bit microprocessor to the market

  • 1992

    • Toshiba introduces its VHC family featuring high speed, low power and low noise. National Semiconductor joins Toshiba as second source for this product
    • Toshiba markets its R4000 64-bit microprocessor based on MIPS architecture

  • 1991

    • First 2.5" HDD, 90MB*
    • Toshiba develops the world's first 4-megabit NAND-type EEPROM
    • Toshiba introduces the world's fastest Bi-CMOS Logic ICs
    • Toshiba announces its first Neuron Chip, which is the foundation of Echelon's LONWORKS™ Technology
    • Toshiba develops red-light semiconductor laser with the world's highest optical output power
    • Toshiba's CCD imaging technologies wins 1991 EMMY Awards
    • Toshiba begins operations at Display Technology, Inc.
    • Toshiba introduces the world's shortest wavelength VLD at 650 nanometers

  • 1990

    • Ships first HDD using glass media on a single-platter, 40MB 2.5-inch hard drive
    • Toshiba and Siemens announce cooperation in RISC microprocessors with MIPS architecture
    • Toshiba enters RISC Chip business with License for MIPS' R3000/R4000 Series
    • Toshiba Display Devices (TDD) in Horseheads, New York, becomes wholly owned subsidiary of TAEC
    • Toshiba becomes one of the first Rambus licensees
    • Toshiba develops prototype VLD with the world's shortest wavelength of 638 nanometers. Toshiba develops new LCD for notebook computers
    • Toshiba's Gate Turn-Off Thyristor's receives R&D 100 Award
    • Toshiba announces its support for Echelon's LON Neuron™ Chip

  • 1989

    • Establishes voluntary social and environmental program aimed for the betterment of humans worldwide and the health of the planet
    • Display Technology, Inc., (DTI) a joint venture between Toshiba Corporation and IBM Japan, LTD, established to manufacture thin film transistor LCD's
    • Toshiba completes clean room at Sunnyvale facility for custom development and metallization of Gate Arrays
    • Toshiba invents NAND Flash technology
    • Toshiba develops resist asher by ultraviolet ozone for large LCDs
    • Toshiba markets Visible-Light Emitting Laser Diodes (VLDs) with the world's shortest wavelength of 660 nanometers

  • 1988

    • Toshiba America, Inc.'s Electronic Components business sector (TAEC) relocates to Irvine, CA.
    • Toshiba begins using Impregnated Cathode in its Color Picture Tubes
    • Toshiba announces improved high-speed CMOS Logic family of devices
    • Toshiba develops 4 megabit DRAM
    • Toshiba introduces new monochrome high-contrast LCD

  • 1987

    • Toshiba produces world's first SAW Filter for cordless phone
    • Toshiba produces world's first UHF SAW filter for satellite receiver

  • 1986

    • First 3.5" HDD, 26MB*
    • Toshiba Display Devices (TDD), in Horseheads, NY began production of 19/20" Color Picture Tubes.
    • Toshiba introduces world's first wide-band SAW Filter for TV-IF

  • 1985

    • Toshiba develops 1-megabit CMOS dynamic RAM.
    • Toshiba introduces world's first SAW Resonator Filter for pagers

  • 1984

    • Introduction of INVAR Shadow Mask and first 15" Full Square Color Display Tube Production.

  • 1983

    • First 5.25" Disk Drive, 27MB*

  • 1982

    • First Full Square color picture production For TV

  • 1981

    • First 8" Disk Drive, 48MB*

  • 1980

    • Establishes industry leadership with the world's first 10.5-inch HDD and begins the Eagle product line*
    • Toshiba produces world's first SAW Resonator for VCR RF modulator

  • 1978

    • Toshiba begins production of the first Mini-Neck Color Picture Tube

  • 1977

    • Toshiba produces first SAW Filter for TV-IF, at the Himeji Factory in Japan

  • 1973

    • Toshiba begins research and development on SAW devices

  • 1972

    • Toshiba begins production of the first Blackstripe Slit Mask Color Picture Tube

  • 1969

    • Delivers first Hard Disk Drive, 14" Form Factor*
    • Fukaya Works opens for CRT's for TV and Monitors

  • 1967

    • Enters the HDD industry with 14-inch HDDs

  • 1965

    • Toshiba America, Inc. establishes Electronics Components business sector to market Toshiba components in North America
    • Himeji Works Production of 19" Color Picture Tube.

  • 1958

    1958 Square Color Picture Tube
    • Toshiba produces the industry's first Square 17-inch Color Picture Tube.

Note: All firsts and claims made are as of the release date.

·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.