Contact us

A new window will open A new window will open

AC-DC Flyback Power Supplies

AC-DC flyback converters, which consist of a small number of components, are used for power supply applications with a wattage of less than 100 W such as adapters for notebook PCs and other mobile devices. Toshiba offers low-loss MOSFETs with a VDSS of 800 V ideal for flyback applications.

Block Diagram

Click on the colored blocks to view recommended products.

フライバック型AC-DC電源の回路例

PFC MOSFET Main Switch PFC Controller ICs Blocking Diode Photocoupler Gate Driver Secondary Rectification

Documents

Whitepaper

Whitepaper
Name Outline Date of issue
Describes the features of the DTMOSV series and the improvements from the previous series 9/2017

user registration

  • DTMOS Applications (Noise Reduction)
Describes the mechanism of noise generation and noise reduction techniques coming soon

Application Note

Application note
Name outline Date of issue
Provides hints and tips based on simulation results to help you reduce the chip temperature of discrete semiconductor devices. 01/2018
The high dv / dt between the drain and the source of the MOSFET can cause problems and explain the cause of this phenomenon and its countermeasures. 12/2017
Describes mechanism of avalanche phenomenon, I will explain durability and countermeasures against it 12/2017
describes how to reduce the chip temperature of discrete semiconductor devices. 12/2017
describes how to calculate the temperature of discrete semiconductor devices. 12/2017
discusses temperature derating of the MOSFET safe operating area. 12/2017
When a rapidly rising voltage is applied between the drain and source of the MOSFET,the MOSFET may malfunction and turn on, and its mechanism and countermeasures will be explained. 12/2017
Describes the guidelines for the design of a gate driver circuit for MOSFET switching applications and presents examples of gate driver circuits 11/2017

user registration

Describes current imbalance in parallel MOSFETs and the mechanism of parasitic oscillation 11/2017

user registration

Describes the oscillation mechanism of MOSFETs for switching applications 11/2017

user registration

Describes thermal equivalent circuits, examples of channel temperature calculation and considerations for heatsink attachment 2/2017
Describes planar, trench and super-junction power MOSFETs 11/2016
Describes the absolute maximum ratings, thermal impedance and safe operating area of power MOSFETs 11/2016
Describes electrical characteristics shown in datasheets 11/2016
Describes how to select power MOSFETs, temperature characteristics, the impacts of wires and parasitic oscillation, avalanche ruggedness, snubber circuits and so on 11/2016

Video


  • Circuit Overview

    When the switch is closed, the primary inductance of a transformer stores energy. When the switch is opened, the stored energy is transferred from the transformer to the output load. Therefore, the output voltage is not a function of the transformer turns ratio.

    The output voltage is determined by the on/off ratio of the transistor, the primary inductance of the transformer, and the load resistance (R):
     

    Vo={√(R/2Lp)[Ton/√(Ton+Toff)]}Vin
    where, Lp is the primary inductance, Ton and Toff are the "on" and "off" periods of the transistor, and R is the load resistance.



    A flyback converter consists of a small number of parts. However, since the core size must be increased to obtain high power output, flyback converters are utilized only for low-wattage power supply applications.

    Compared with a forward converter, a flyback converter can dispense with an output inductor and a flywheel diode, making it suitable for low-cost power supplies.

    Since the flyback converter does not have an output inductor, it provides excellent load transient response.

    For high-frequency switching, a small, lightweight transformer can be used.

 *Click the headline to open it

  • Operation

    When Q1 is turned on, energy is stored in the primary winding. When Q1 is turned off, it is transferred to the secondary winding and supplies the output load.

    1. Q1 ON/Q2 OFF  (Ton)

    A voltage (Vdc) is applied across LP.

    The primary current in the transformer increases as shown according to its current gain.

    dip/dt=(VS-VDS1)/Lp
    where, VDS1 is the Q1 voltage, and Lp is the primary inductance.

    Hence, the peak current at the end of the "on" state is calculated as follows:

    Ip=(VS-VDS1)Ton/Lp

    The electromagnetic energy stored in the primary winding is calculated as:

    E=Lp × Ip2 /2

    2. Q1 OFF/Q2 ON  (Tr)

    The voltage polarity of the secondary winding reverses

    As a result, the energy stored in the secondary winding is released. At this time, the secondary current linearly decreases as shown in the following equation:

    dIs/dt=VOUT/Ls  where, Ls is the secondary inductance.

    If Is becomes zero before Q1 is turned on again, all the energy stored in the primary (E) is delivered to the output load. The power supplied to the output load is calculated as follows:

    P=E/T=[(VS-VDS1)Ton2/(2T×Lp) ≈ (VS×Ton)2/(2T×Lp)

    Then, since the power delivered to the load is Vo2/RL, VOUT is calculated as follows:

    (VS×Ton)2 / (2T/Lp) = VOUT2/RL
    VOUT = (VS×Ton)√[RL/(2T×Lp)]

 *Click the headline to open it

Contacts

If you have any questions, click one of these links:

Technical queries
Questions about purchasing, sampling and IC reliability
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.