Contact us

A new window will open A new window will open

Toshiba Expands Line-up of New-generation Transistor Arrays

March 13, 2017

New-generation Transistor Arrays

TOKYO–Toshiba Corporation's (TOKYO: 6502) Storage & Electronic Devices Solutions Company today announced that it is meeting customer requirements for a wider variety of output and input methods and functions by adding 19 products to its line-up of new-generation transistor arrays equipped with DMOS FET[1] outputs. The new devices join the 37 products in the TBD62xxxA series, which have found wide application in areas including motors, relays, LEDs, and level shifters for control communication lines. Sample shipments start today, and the new products will be introduced sequentially.
 

Products currently in mass production are mainly High-active (H-active) type products in which output is turned on if H level is input. Toshiba is now adding Low-active (L-active) products in which output is turned on if L level is input. L-active products are well suited to level shifters for control communication lines in industrial equipment, amusement equipment and home appliances.

In addition, Toshiba is also adding to the line-up the TBD62381A series, which realizes low power consumption by modifying characteristics of in-line products TBD62083A series.

Alongside TBD62089APG, a sink-output type transistor array equipped with D-type Flip Flop circuits (8-bit type) in the input, which has been in mass production since January, Toshiba has also added a source-output type transistor array, TBD62789APG, in response to demand from the amusement and industrial equipment field.

Combining sink-output type and source-output type transistor arrays is suitable for supplying power source and constructing ON and OFF control systems in electric lighting applications.

Main Features of New Products

1. Offers products with two input types according to the needs

H-active products input control signals directly from the CPU (for the motor drive, the relay drive, the LED drive, etc.), while L-active products input control signals via an open drain configuration circuit (for level shift in the control communication line, etc.).

2.

Offers two output type products: the source output type used for switching power supply and the sink output type used for ON / OFF control. Dynamic control of the LED matrix is possible by combination of source output and sink output.

3. High efficiency drive

New-generation transistor arrays, “TBD62XXX” series cut power loss by about 40% [2] compared to preceding TD62XXX series.

4. High-voltage, large-current drive

Absolute maximum output rating is 50V/0.5A

5. Packages for various applications

The line-up includes DIP packages, where there is strong demand for the hobby goods, amusement and industrial equipment fields; SOL packages that support surface mounting; and small SSOP packages (0.65 mm pin pitch) suitable for saving space in set products.

Applications

Industrial equipment (vending machines, banking terminals such as ATMs, office automation equipment, and factory automation equipment), amusement equipment (pachinko and slot machines), home appliances (air-conditioners and refrigerators), etc.

Product Line-up

Part number Output type No. of
Channels
Output Output ON resistance Common diode Input type Package Sample release schedule Previous products
TBD62304A PG Sink 7ch 50V
0.5A
2Ω
(typ.)
- L-active
(buffer)
DIP16 March 2017 TD62304APG
FNG SSOP16 TD62304AFNG
FWG SOL16 TD62304AFG
TBD62387A PG 8ch 50V
0.5A
2Ω
(typ.)
Built-in L-active
(buffer)
DIP20 March 2017 TD62387APG
FNG SSOP20 TD62387AFNG
TBD62384A PG 8ch 50V
0.5A
2Ω
(typ.)
- L-active
(buffer)
DIP18 April 2017 TD62382APG
TD62384APG
FNG SSOP18 TD62382AFNG
FWG SOL18 TD62382AFG
TD62384AFG
TBD62381A PG 8ch 50V
0.5A
1Ω
(typ.)
- H-active
(inverter)
DIP18 March 2017 TD62381PG
FNG SSOP18 TD62381FNG
FWG SOL18 TD62381FG
TBD62781A PG Source 8ch 50V
0.5A
1.6Ω
(typ.)
- H-active
(buffer)
DIP18 April 2017 TD62781APG
FWG SOL18 TD62781AFG
TBD62785A PG 8ch 50V
0.5A
1.6Ω
(typ.)
- L-active
(inverter)
DIP18 May 2017 TD62785PG
FWG SOL18 TD62785FG
TBD62786A PG 8ch 50V
0.5A
1.6Ω
(typ.)
Built-in L-active
(inverter)
DIP18 June 2017 TD62786APG
FNG SSOP18 TD62786AFNG
FWG SOL18 TD62786AFG
TBD62789A PG 8ch 50V
0.5A
2Ω
(typ.)
Built-in H-active
(data storage function)
DIP20 March 2017 -

[1]: DMOS FET: Double-Diffused MOSFET

[2]: In the condition of Ta=25℃ and IOUT is 200mA.

Follow the link below for more on Toshiba Transistor Arrays.

https://toshiba.semicon-storage.com/ap-en/product/linear/transistor-array.html

Customer inquiries:

Mixed Signal IC Sales and Marketing Department
Tel: +81-44-548-2826
https://toshiba.semicon-storage.com/ap-en/contact.html

*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.