Contact us

A new window will open A new window will open

Toshiba Expands Line-Up of Photorelays in DIP8 Packages by Adding Mid-Voltage Range Products

May 16, 2017

Company enhancing line-up of large current products with drive current above 1A as replacements for mechanical relays in industrial applications.

DIP8

TOKYO–Toshiba Corporation's (TOKYO: 6502) Storage & Electronic Devices Solutions Company today announced the launch of new two mid-voltage products, the 100V "TLP3823" with a 3A drive current, and the 200V "TLP3825" with a 1.5A drive current, additions to its line-up of large current photorelays to replace mechanical relays. Mass production shipments start today.
 

Alongside Toshiba’s current 60V "TLP3547" with a 5A drive current, the new products with drive currents higher than 1A will extend the range of photorelay application.
 

Recent years have seen accelerated replacement of mechanical relays with photorelays. Toshiba is supporting and promoting this shift by applying its latest trench MOSFET, 8th generation UMOS, to realize output currents exceeding 1A.

Unlike mechanical relays, photorelays have no physical contacts subject to wear and tear, an advantage that contributes to set reliability. Use of photorelays also supports development of smaller and thinner products. Toshiba’s new photorelays also offer the advantage of a guaranteed pulsed on-state current that is three times larger than continuous on-state current, securing a bigger margin for safety design.

The latest Gartner market report recognizes Toshiba as the leading manufacturer of optocouplers by sales in 2015 and 2016, with a 23% by sale-based market share in CY2016. (Source: Gartner “Market Share Semiconductor Devices and Applications Worldwide 2016”,  30 March 2016).

Toshiba will continue to deliver products that meet the needs of customers by promoting the development of a diverse portfolio of photocouplers and photorelays tailored to market trends.

Features

TLP3823:

VOFF=100V(min), ION=3A(max), ION(pulse)=9A(max)@t=100ms, Duty=1/10

TLP3825:

VOFF=200V(min), ION=1.5A(max), ION(pulse)=4.5A(max)@t=100ms, Duty=1/10

Main Applications

  • Industrial equipment
  • General purpose inverters
  • Heating, Ventilation and Air Conditioning (HVAC)
  • Thermostats
  • Building automation equipment
  • Semiconductor testers (Memory, SoC, LSI)
  • Various test equipment
  • Replacement of mechanical relays

Main Specifications

(@Ta=25℃)

Part Number Absolute Maximum Rating On-state Resistance Trigger
LED
current
IFT
max
(mA)
 
Off-State Current
IOFFmax
(µA)
@VOFF
(V)
Turn-On
time
tON
typ.
(ms)
Turn-Off
Time
tOFF
typ.
(ms)
Package
Off-state
output
terminal
Voltage
VOFF
(V)
On-state
Current
ION
(A)
On-state
current
(pulsed)
IONP
(A)

Isolation voltage
BVS
(Vrms)
RON
typ.
(mΩ)
RON
max
(mΩ)
TLP3547 60 5 15 2500 22 50 5 1
(@VOFF=
60(V))
2.5 0.1 DIP8
TLP3823[1] 100 3 9 2500 60 150 5 1
(@VOFF=
100(V))
1.5 0.1
TLP3825[1] 200 1.5 4.5 2500 250 500 5 1
@VOFF=
200(V))
0.25 0.1

Notes

 [1] New products.

Follow the link below for more on the new products and the Toshiba photorelay line-up.

https://toshiba.semicon-storage.com/ap-en/product/opto/photocoupler/photorelay.html

Customer Inquiries:

Optoelectronic Device Sales & Marketing Dept.
Tel: +81-3-3457-3431
https://toshiba.semicon-storage.com/ap-en/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is correct on the date of the announcement but is subject to change without prior notice.

·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.