Contact us

A new window will open A new window will open

What is the difference between small-signal transistors and power transistors?

There is no internationally uniform classification distinguishing between small-signal and power transistors. Toshiba refers to transistors with a power dissipation (PC) of 1 W or less as "small-signal transistors," and those with a PC higher than 1 W as "power transistors."

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.