Contact us

A new window will open A new window will open

NAND Flash Memory

Toshiba, the Inventor of Flash Memory

Back in 1984, Toshiba developed a new semiconductor memory, Flash Memory, and by doing led the industry, and its competitors, into the next generation.

Today the international de facto standard, NAND Flash Memories have realized an immense range of applications that include Memory Cards, Solid-State Drives (SSDs), and even industrial equipment.
As the total volume of information continues its exponential growth, demand for storage units using NAND Flash Memories will grow with it. In order to meets these market needs, Toshiba has made major investments in plant and equipment at its Yokkaichi memory fab, and is resolutely committed to develop new products.
This brochure highlights Toshiba's NAND Flash Memory and other Memory Solutions.

Toshiba's NAND flash memory and Applications

Documents

Catalog

Video Clips

Features of NAND Flash Memory

NAND flash memory is suitable for storing large amounts of data.

  • Fast storage of large files
  • Fast write and erase rates
  • Low per-bit cost
  • Easily extendable using the NAND Flash Memory interface
  • Extensive product portfolio to meet diverse needs
    • Products with the standard HS-MMC interface
    • Offers products with the high-speed UHS-I and UHS-II SD bus interfaces
    • Available as SD Memory Cards with unique features

Yokkaichi Operations, the manufacturing site for NAND Flash Memories

Photo of Toshiba Yokkaichi Operations as seen from the sky Click to enlarge

Toshiba manufactures all its NAND Flash Memories at its Yokkaichi Operations in order to maintain their quality.
On September 9, 2014, Phase 2 of Fab 5 and the newly built Fab 2 were inaugurated.
In order to meet growing demand for memory chips, Toshiba has increased its plant investments in expanding manufacturing capacity and accelerating the development and production of next-generation memories.

Contacts

If you have any questions, click one of these links:

Technical queries
Questions about purchasing, sampling and IC reliability
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.