Contact us

A new window will open A new window will open

SLC NAND Flash Memory

The Toshiba SLC NAND supports customers' businesses with an extensive lineup of technologies

For a wide application

To meet diverse customers' application needs, Toshiba offers SLC* NAND flash memory products with a wide range of capacity points and multiple packaging options. The high read/write performance and write endurance of the Toshiba SLC NAND make it a superb choice for a broad spectrum of commercial and industrial applications. SLC NAND also provides a significant cost advantage compared with NOR flash memory.

Toshiba, the inventor of flash memory, has led the world in using successive generations of fabrication processes to steadily enhance its performance. Toshiba also offers BENAND™ that incorporates error checking and correction (ECC) and Serial Interface NAND that provides a serial peripheral interface for NAND flash interfacing. Thus, you can select the optimal SLC NAND according to your host ECC and memory interface requirements.

* SLC: single-level cell
* BENAND: Built-in ECC NAND
   BENAND is a trademark of Toshiba Corporation.

 

SLC NAND Flash Memory Lineup

- The Toshiba SLC NAND lineup includes three categories of products.
- You can choose a product that best fits your needs accordingly to the ECC capability and the memory interface of the host chipset.

The high read/write performance and write endurance of the Toshiba SLC NAND make it a superb choice for a broad spectrum of commercial and industrial applications.

SLC NAND Block Diagram

BENAND™ is a NAND flash memory that incorporates ECC logic. BENAND™ eliminates the need for a host processor to perform ECC, making it possible to utilize the latest 24-nm SLC NAND regardless of whether the host processor has an adequate ECC capability.

BENAND Block Diagram

Serial Interface NAND provides a commonly used six-pin Serial Peripheral Interface (SPI) for flash memory interfacing and is offered in small WSON, SOP and BGA (*)packages.

* BGA package is under planning

Serial Interface NAND Block Diagram
* The ECC logic in Serial Interface NAND can be enabled and disabled by the customers.

Product List

List of SLC NAND
You can search the entire list of SLC NAND, based on characteristics.

Contacts

If you have any questions, click one of these links:

Technical queries
Questions about purchasing, sampling and IC reliability
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.