Contact us

A new window will open A new window will open

Secure firmware rotation

Updating firmware of shipped devices has become technically easy. However, updating of device firmware in the field poses the risk of rewriting with malicious firmware. A device rewritten with malicious firmware may not only stop operating correctly but is also a vulnerability that may be exploited to attack other systems. Secure microcomputer firmware rotation is a feature with the following functions to detect unauthorized writing to a flash memory.

  • Falsified firmware is detected on boot.
  • When firmware is in an abnormal state, the operation stops autonomously to prevent secondary damage.
  • Firmware has a flash memory with a two-side configuration, and writing to the side under execution is prohibited.

Secure firmware rotation

Video

White paper

New technology to protect firmware against falsification and safely update IoT devices

Download

Contacts

If you have any questions, click one of these links:

Technical queries
Questions about purchasing, sampling and IC reliability
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.