Contact us

A new window will open A new window will open

USB (Universal Serial Bus)

USB is a very popular serial interface especially for PCs. As well known, the interface is used to connect to a PC such equipments as a keyboard, a mouse, a printer, a Flash memory, a hard disk drive, a speaker, and so on. USB has several speed versions, Low-Speed (1.5Mbps), Full-Speed (12Mbps), High-Speed (480Mbps) and so on. Toshiba TX03 series microprocessors support USB Full-Speed.

A hierarchical structure is applied to USB interface. One “Host” dominates many “Devices” in a network. For example, a PC is a Host, and Devices are any apparatuses which are connected to the PC through USB cables, like a keyboard, a mouse and so on.

usb01

USB has a remarkable feature of plug-and-play. Switching off a PC is unnecessary when USB Devices are connected or removed. This is one of the reasons USB has become so popular.

The cable of USB has 4 wires; VDD, GND, signal D+, and signal D-. D+ and D- are complementary values each other for one transferred data. In the case that D+ is high and D- is low, the data is called “Differential 1”. And D+ is low and D- is high, “Differential 0”.The data format of USB is NRZI (non-return to zero inverted). This format defines data “1” when no change occurs in one clock interval, and data “0”, either high-to-low or low-to-high change occurs.

usb02_e

USB does not have any clock lines. So the Host and the Driver have to synchronize each other. 8 bit SYNC codes are transferred to synchronize a receiver to a transmitter in USB Full-Speed.

Product List

TX03 series products incorporating a USB interface are displayed.

Contacts

If you have any questions, click one of these links:

Technical queries
Questions about purchasing, sampling and IC reliability
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.