require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Select Product Categories
Select Application
Find everything you need for your next product design. Simply select an application and click through to the block diagram to discover our semiconductor solutions.
New Products / News
Air cleaners were developed due to air pollution that occurred during the period of high economic growth. Today, it is often used to remove so-called air pollutants. However, it is increasingly used for hay fever and PM2.5, which have recently become a social issue, and filter performance and fan capacity are improving. And what has been increasing in recent years is the linkage function with smartphones and smart speakers. Sensors detect the condition of air. These sensors allow you to check the content of PM2.5, VOCs (volatile organic compounds) and other substances with dedicated applications and voice. They also allow you to switch the operation of air cleaner from a remote location or from outside. In addition, air cleaners have been developed that use artificial intelligence (AI) and clouds to realize automatic operation suitable for users by learning how to use the users and to fit their homes, and that also provide functions that link air conditioners and air cleaners to adjust room air to the best condition. To realize these functions, optimization of power supplies for MCUs and wireless SoCs, improvement of motor control efficiencies and sensing circuit designs are important. Toshiba offers ultra-low-noise CMOS operational amplifiers, power management ICs such as LDO regulators, and intelligent power ICs, contributing to the realization of evolving air cleaners.