require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Select Product Categories
Select Application
Find everything you need for your next product design. Simply select an application and click through to the block diagram to discover our semiconductor solutions.
New Products / News
With the economic development of emerging countries and the growing demand for data centers, the demand for air conditioners is growing. For Household air conditioners, regional characteristics, such as climatic, cultural, and incomes levels, and energy-saving, low-cost, and reduced CO2 emissions, as well as connectivity as smart home appliances are keys to product design. For industrial air conditioners, especially for data centers, it is important to achieve proper temperature control in a heat-generating environment that increases as the amount of data handled increases and the performance of equipment increases, as well as appropriate humidity control for preventing dew condensation on computer components and preventing static electricity with low power consumption. To solve these problems, power supply efficiencies and sensing circuit designs are important. Toshiba's lineup of MOSFETs, intelligent power ICs, operational amplifiers, and other products that incorporate latest technologies are contributing to enhancing air conditioning performance without increasing power dissipation.