require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Select Product Categories
Select Application
Find everything you need for your next product design. Simply select an application and click through to the block diagram to discover our semiconductor solutions.
The function of blood glucose meters has been advancing year by year, making easier and more accurate to measure. We have also begun to include additional functions, such as recording blood glucose levels measured on a daily basis and interworking with personal computers and smartphones. Toshiba has a lineup of low-noise CMOS operational amplifiers to amplify sensor signals to measure blood glucose levels with high accuracy, LDO regulators to enable the efficient operation of complex electronic circuits inside blood glucose meters, and TVS diodes (ESD-protection diodes) to protect blood glucose meters from external static electricity. These semiconductors are installed in a compact, lightweight package, contributing to the reduction of board space in order to increase the precision and functionality of blood glucose meters.