require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Select Product Categories
Select Application
Find everything you need for your next product design. Simply select an application and click through to the block diagram to discover our semiconductor solutions.
New Products / News
A MOSFET with high withstand voltage and low on-resistance is suitable for the power module. By keeping the on-resistance low, heat generation and current consumption can be minimized, and loss can also be reduced. Toshiba's Power MOSFET Series uses high heat dissipation packages to further reduce heat generation. The transistor output photocoupler is used for voltage feedback to the primary side in the power supply module circuit. Signal transmission at different potentials is required on the primary and secondary sides, and signal path isolation can be easily and reliably realized by using an optical coupling method photocoupler. When using photocouplers, it is essential to observe the safety standards established in each country. Toshiba Photocouplers have been approved by UL1577, VDEs: EN60747-5-5, EN62368-1, and others.
Examples of typical recommended products are listed below, and also provide a link to the online distributor inventory search page to buy the product.
Toshiba has provided the Switched Mode Power Supply Library to support power supply designs such as DC-DC power supply. In addition, the Reference Design Center publishes examples of the design of various power supply circuits, providing design ideas for high efficiency in various power supply circuits. Both of them can be used free of charge, so please use them as a help in designing the power supply.
Switched Mode Power Supply Library
Easily select the optimal circuit and MOSFETs. Downloads circuit data that can be used in OrCAD®, LTspice® environments.
Reference Design Center
Releasing various reference designs that can be used for end equipment.
Toshiba offers super-junction MOSFET series suitable for high-output power supply applications and D-MOS (double-diffused) MOSFET series suitable for low-output power supply applications.
Toshiba's portfolio of isolators/solid state relays includes photocouplers, solid-state relays and fiber-optic transmission modules. Toshiba's photocouplers help improve the safety, cut the power consumption and reduce the size of end products.