require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Select Product Categories
Select Application
Find everything you need for your next product design. Simply select an application and click through to the block diagram to discover our semiconductor solutions.
New Products / News
Uninterruptible power supplies (UPSs) are necessary for the continued operation of equipment in the event of a power failure. By supplying power that was normally charged from commercial power to the battery, the equipment can be safely shut down, backed up, and protected when power failure happens by typhoons and lightning strikes for example. Power supply failures cause equipment failure, data loss, file collapse, etc., and the restoration of these system failures requires enormous time and expense. In addition, network system shutdowns can lead to not only physical damage, but also losing of business opportunities and credibility. UPS are indispensable to prevent such situations. In recent years, prices are cheper, and users who record video on high-capacity HDDs at all times, players of online games, and individual online traders are becoming increasingly familiar. High-efficiency performance is strongly required for large-capacity types, while small-and medium-capacity types also require performance such as compactness and light weight. Toshiba's MOSFET having new process technology with a high heat dissipation package, contributes to the realization of a highly efficient power supply, and offering performances suitable for power supply circuitry and output stages of equipment. To maintain stable operation in harsh environments, Toshiba's photocouplers can be used to solve problems.
* Company names, product names, and service names may be trademarks of their respective companies.