Contact us

在新窗口打开 在新窗口打开

东芝推出8TB企业容量级硬盘驱动器

2017年04月06日

为3.5英寸SATA接口阵容增添大容量型号

MG05 series

东京--东芝公司(TOKYO:6502)旗下存储与电子元器件解决方案公司今天宣布,已为其3.5英寸[2]外观企业容量级硬盘驱动器(HDD)新增8TB[1] SATA型号MG05系列。出货即日起启动。  


随着物联网(IoT)扩展和云服务普及,所生成和积累的数据量也在持续增加,而云数据中心及其存储系统则不断需要更高容量、更高性能的硬盘驱动器。  


为满足上述需求,新型8TB型号提供的最大容量较之前MG04系统的6TB型号增加近33%。此外,其持续数据传输率也提高近12%[3],达到230MiB/秒,以及MTTF[5]提升约42%[4],达到200万小时。这些容量、速率和可靠性方面的改进有助于降低系统的总拥有成本(TCO)。  


新型硬盘驱动器支持业界标准的原生4K和512e高级格式扇区技术,可用于最新一代服务器和存储系统,而且还适用于需要512扇区长度且利用写入对齐(aligned-write)环境的传统应用。  


最新IDC市场报告[6]将东芝视为相比2015年在2016年发展最快的硬盘驱动器供应商。同样,该报告还发现东芝在2016年第四季度的市场份额为24%(为台数为度量标准)。


2017年2月,东芝的近线企业级硬盘驱动器的累计产量超过1,000万台。东芝将继续开发和提供满足客户需求的产品。  

注释

[1] 容量定义:东芝将1兆字节(TB)定义为1,000,000,000,000字节。但是,计算机操作系统报告的存储容量利用2的方幂定义,即1GB = 230 = 1,073,741,824字节,因此显示的存储容量变小。可用存储容量(包括不同媒介文件)会基于文件大小、格式、设置、软件和操作系统而异,例如Microsoft操作系统和/或预安装的软件应用或媒体内容。实际格式化内容也可能有所差异。
[2] “3.5英寸”指的是硬盘驱动器的外观尺寸。它们不代表驱动器的实际尺寸。
[3] MG04系列(205MiB/秒)与MG05系列(230MiB/秒)之间比较
[4] MG04系列(140万小时)与MG05系列(200万小时)之间比较
[5] 平均故障间隔时间(MTTF)并非产品寿命的保证或估计值;它是与大量产品的平均故障率相关的统计值,这些产品可能无法准确反映实际运行情况。产品的实际运行寿命可能与平均故障间隔时间有所差异。
[6] 2016年发展最快的硬盘驱动器供应商(相较于2015年),基于IDC《2016年第四季度硬盘驱动器全球出货结果与四季度预测更新》(2017年2月 – 文件编号US42306617),以收入和台数为度量标准评估。

欲了解更多关于东芝企业级硬盘驱动器,请访问:

https://toshiba.semicon-storage.com/ap-en/product/storage-products/enterprise-hdd.html

客户问询:

日本总部
存储产品销售&市场部
电话:+81-3-3457-2445

中国地区
存储产品销售&市场部(Storage Product Sales & Marketing)
上海:021-6139-3888 / 深圳:0755-2399-6897

Information in this document, including product prices and specifications, content of services and contact information, is correct on the date of the announcement but is subject to change without prior notice.

·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.