Contact us

在新窗口打开 在新窗口打开

东芝推出集成64层3D闪存的NVMeTM SSD

2017年05月31日

东芝存储公司

采用薄型单面规格、容量高达1024GB[1]的XG5系列客户级SSD

NVMe(TM) SSD Using 64-Layer, 3D Flash Memory

东京—东芝存储公司(以下简称为东芝)今日宣布推出XG5系列,这是一款集成64层3D闪存,采用单面规格设计,用户容量最高可达1024GB的全新NVM ExpressTM (NVMeTM)SSD阵容。东芝于今日起针对OEM客户进行小规模样品出货,并将于今年第三季度(7-9月)开始逐步增大出货规模。

此款全新SSD系列搭载了东芝最新的64层3bit-per-cell TLC(1个存储器储存单元可存放3比特的数据)BiCS FLASHTM存储器,利用PCI EXPRESS®(PCIe®)Gen3 x 4通道以及SLC缓存的特性,能提供3000MB/s的顺序读取[2]和2100MB/s顺序写入[2]的传输性能。而且,对比东芝现有产品[3],此款SSD系列具有更高电力效率(单位功耗的读写性能),待机模式时的功耗降低了50%以上,实现了3mW [4]以下的待机功耗。

此款SSD提供三种容量:256GB、512GB和1024GB。全部采用M.2 2280[5]单面规格。十分适用于重视性能的超级移动电脑等一系列领域的广泛应用。

XG5系列SSD将于2017年5月30日至6月3日在台湾台北市举行的“台北国际电脑展”进行展出。

东芝将运用先进的闪存技术继续增强其SSD存储解决方案以满足多样化的市场需求。

*PCIe®和PCI EXPRESS®是PCI-SIG的注册商标。

*NVMe和NVM Express是NVM Express公司的商标。

*本文提及的所有其它公司的名称、产品名称和服务名称可能是其各自公司的商标。

[1] 容量定义:东芝定义1千兆字节(GB)为1,000,000,000字节。而计算机操作系统使用2的幂数来标示存储容量,其定义1GB=230字节=1,073,741,824字节,因此会显示较少的存储容量。根据不同的文件大小、格式、设置、软件和操作系统,可用存储容量(包括各种媒体文件示例)将存在差异,如微软操作系统和/或预装软件应用程序或媒介内容。实际的格式化容量可能存在差异。

[2] 该性能是根据东芝测试标准,使用128KiB单元顺序访问测得的XG5 1024GB型号产品的顺序读取和顺序写入性能。根据不同的测试环境,读写条件以及负载,其性能存在差异。东芝定义1兆字节(MB)为1,000,000字节,1千位二进字节(KiB)为210字节或1,024字节。

[3] XG3系列

[4] 该性能是根据东芝测试标准,在非工作电源状态中链路电源管理状态L1.2的条件下测得的功耗性能。

[5] M.2 2280-S2

客户问询:

日本总部
SSD销售与市场营销部
电话:+81-3-3457-3432
https://toshiba.semicon-storage.com/ap-en/contact.html


中国地区
存储器件市场部(Memory Marketing)
上海:021-6139-3888/深圳:0755-2399-6897

Information in this document, including product prices and specifications, content of services and contact information, is correct on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.