Contact us

在新窗口打开 在新窗口打开

东芝推出新一代15,000 RPM企业级2.5英寸硬盘驱动器新系列

2017年06月13日

东芝公司

可提供最大容量达900GB

AL14SX Series

东京-- 东芝公司(TOKYO:6502)旗下存储与电子元器件解决方案公司今日宣布推出AL14SX系列,该新系列为其企业级硬盘驱动器(HDD)产品阵容中的最新产品,它们适用于关键任务服务器和存储应用。样品发货即日启动。
 

AL14SX系列15,000 RPM 2.5英寸[1]驱动器采用12Gbit/s[2] SAS接口。可选型号包括采用先进格式扇区技术的4K native (4Kn)型号和512 emulation (512e)型号,以及针对旧版应用程序和管理程序环境进行了优化的512 native (512n)型号。AL14SX系列为客户多样化的应用提供适当的选择。
 

AL14SX系列提供300GB、600GB和900GB存储容量。与上一代600GB产品AL13SX系列相比,900GB[3]型号的最大容量增加50%。此外,4Kn和512e型号的持续数据传输率提高了约19%,提升至290MiB/s[4],而功率效率(W/GB)提高了约28.7%。新产品在容量、速度和节能方面的改善有助于降低服务器和系统的总体拥有成本(TCO)。

客户还可以选择支持清理即时擦除(SIE)的型号,使磁盘上记录的数据实现快速失效,支持高效处理和重用。

[1] “2.5英寸”指硬盘驱动器的外形。并不表示驱动器的实际尺寸。

[2] 根据主机设备、读取和写入条件以及文件大小情况,读写速度可能存在差异。

[3] 容量定义:东芝定义1兆字节(MB)为1,000,000字节,1千兆字节(GB)为1,000,000,000字节,1太字节(TB)为1,000,000,000,000字节。而计算机操作系统使用2的幂来报告存储容量,其定义1GB = 230 = 1,073,741,824字节,因此显示更少的存储容量。根据不同的文件大小、格式、设置、软件和操作系统,可用存储容量(包括各种媒体文件示例)将存在差异,如微软操作系统和/或预装软件应用程序或媒介内容。实际的格式化容量可能存在差异。

[4] 1千字节(KiB)代表210或1,024字节、1兆字节(MiB)代表220或1,048,576 字节、1千兆字节(GiB)代表230或1,073,741,824字节。

欲了解有关该新产品及东芝企业级硬盘的更多信息,请访问:

https://toshiba.semicon-storage.com/cn/product/storage-products/enterprise-hdd.html

客户问询:

存储产品事业部
https://toshiba.semicon-storage.com/cn/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is correct on the date of the announcement but is subject to change without prior notice.

·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.