Contact us

在新窗口打开 在新窗口打开

东芝存储器株式会社推出采用64层3D闪存的客户级SATA SSD

2017年08月08日

东芝公司

3D Flash Memory

东京-东芝存储器株式会社作为存储器解决方案的世界领导者,今日宣布推出SG6系列,这是一款全新阵容的客户级SATA SSD,它采用了东芝存储器株式会社先进的64层3bit-per-cell TLC(1个存储器存储单元可存放3比特的数据)BiCS FLASH™存储器。东芝存储器株式会社于今日起针对PC OEM客户进行小规模样品出货,并将从今年第四季度(10-12月)开始逐步扩大出货规模。
 

全新SG6系列SSD采用频宽6.0Gbit/s 的SATA 3.3规格,顺序读取和顺序写入的传输性能分别高达550MB/s和535MB/s[1]。并且,得益于闪存管理的改进和闪存性能的提升,其运行功耗比前一代产品[2]最高降低40%左右。功耗方面的改进延长了电池运行时间,对于移动计算等许多领域的应用大有裨益。
 

此款SSD系列提供三款容量:256GB和512GB和1024GB[3]。每款容量都采用两种外形的尺寸规格:用于传统硬盘(HDD)升级换代的2.5型标准规格和用于主流移动电脑的M.2 2280标准规格[4]
 

SG6 SSD系列也支持本公司专有的QSBCTM(Quadruple Swing-By Code)错误修正技术,这种高效率错误修正码(ECC)有助于保障客户的数据免于损毁并提高可靠性,实现高效准确的数据处理。
 

SG6系列将于2017年8月8日至10日在美国加利福尼亚州圣克拉拉市举行的“闪存高峰会议”上进行展出,展台号为#407。
 

*本文所提及的所有公司的名称、产品名称和服务名称可能是其各自公司的商标。


 

注:

[1] 该性能是根据东芝存储器株式会社的测试标准,使用128KiB单元顺序访问测得的SG6系列1024GB型号产品的顺序读取和顺序写入性能。根据不同的测试环境、读写条件以及负载,其性能存在差异。东芝存储器株式会社定义1兆字节(MB)为1,000,000字节,1千位字节(KiB)为210字节或1,024字节。
 

[2] SG5系列。
 

[3] 容量定义:东芝存储器株式会社定义千兆字节(GB)为1,000,000,000字节。而计算机操作系统使用2的幂数来标示存储容量,其定义1GB=230字节=1,073,741,824字节,因此会显示较少的存储容量。根据不同的文件大小、格式、设置、软件和操作系统,可用存储容量(包括各种媒体文件示例)将存在差异,如微软操作系统和/或预装软件应用程序或媒介内容。实际的格式化容量可能存在差异。
 

[4] 256GB和512GB产品的外形尺寸规格为M.2 2280-S2,1024GB产品的外形尺寸规格为M.2 2280-D2。
 

客户问询:

日本总部
SSD销售与市场营销部
电话:+81-3-3457-3432
https://toshiba.semicon-storage.com/ap-en/contact.html


中国地区
存储器件市场部(Memory Marketing)
上海:021-6139-3888/深圳:0755-2399-6897
https://toshiba.semicon-storage.com/cn/contact.html

Information in this document, including product prices and specifications, content of services and contact information, is correct on the date of the announcement but is subject to change without prior notice.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.