Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

Toshiba Announce Near-Infrared 2.1MP CMOS Image Sensor Featuring Iris Recognition Technology

8th October 2015

Higher sensitivity at IR enables advanced security functionality for mobile devices

Toshiba Announce Near-Infrared 2.1MP CMOS Image Sensor Featuring Iris Recognition Technology

Toshiba Electronics Europe has announced its first CMOS image sensor to enable iris recognition, for improved security on mobile devices. The 2.1-megapixel (MP) T4KE1 captures images for recognition with higher sensitivity than conventional CMOS image sensors by omitting the usual colour filter in the pixel structure, which increases sensitivity in the near-infrared (NIR) spectrum.
 

In recent years, mobile devices – smartphones, tablets, laptops and notebook computers – have adopted user authentication systems to protect access and information security. While fingerprint recognition has grown in use, password entry remains the most common approach. Iris recognition is expected to deliver a better solution, as it offers a high degree of protection without the risk associated with lost or misused passwords, and allows the creation of ‘you as the password’ access.
 

The T4KE1 features an optical size of 1/7.3 inch and pixel pitch of 1.12 micrometre BSI. Image output is 60 frames per second (fps) at 1080p (100fps at VGA). Its MIPI* CSI-2 serial interface, widely used in mobile devices, facilitates the sensor’s integration into end products, and a picture flipping function allows output images to be easily flipped both horizontally and vertically.

Toshiba has also designed and provides with the T4KE1, a 5.20mm (x) x 6.00 mm (y) x 4.06mm (z) reference camera module, enabling customers to evaluate use of the sensor in their mobile products. Included with the modules are design information and technical support to help shorten development turnaround time and contribute to creation of thinner, smaller mobile devices.

*MIPI is a licensed trademark of MIPI Alliance, Inc. in the U.S. and other jurisdictions

T4KE1 Mehr

News Links

    

  High Resolution Image (jpg)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.