Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What type of evaluation tools / boards and documentation will be available (specifically to Serdes)?

For 65nm, our serdes reference board is available for customers.
For 40nm, the one will be available in 2nd Qtr of 2015.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.