Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What if the RTL includes FPGA's proprietary IPs?

Toshiba's plan is to replace any proprietary IP with either Toshiba or third party IP and utilizing wrappers in case to replace for certain macros or cells.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.