Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What technology nodes are supported?

Current product offering is based on 65nm and 40nm technology node.  Next generation products are planned for CY2015.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.