Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What is an IPD?

IPD stands for Intelligent Power Device.

An IPD is a monolithic power IC* that integrates on a single chip either power MOSFETs or IGBTs at the output stage and a circuit that controls the output stage.

* For convenience, we also classify some multi-chip ICs as IPDs.

An IPD can directly drive a brushless DC (BLDC) motor.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.