Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

Does the E-Pad (metal frame) exposed on the surface of a high-side IPD have the same potential as GND?

The DIP26 and HSSOP31 packages for our high-voltage IPDs have an E-Pad (metal frame) exposed on the package surface. Its voltage potential is equal to GND.

The circuit, operation and usage of the high-voltage IPD are also described in "High voltage intelligent power device application note“. Please also refer to this document.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.