Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

Is it possible to use the E-Pad (metal frame) exposed on the surface of a high-voltage IPD as a conductive pin?

No. The DIP26 and HSSOP31 packages for our high-voltage IPDs have an E-Pad (metal frame) exposed on the package surface. It must not be used as a conductive pin.

The circuit, operation and usage of the high-voltage IPD are also described in "High voltage intelligent power device application note“. Please also refer to this document.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.