Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

Metals are exposed on the sides of the SSOP30 package for high-voltage IPDs. What voltage potential do they have?

The metals exposed on the sides of the SSOP30 package have the voltage potential shown below.

The metals exposed on the sides of the SSOP30 package

Also see the "High voltage intelligent power device application note“ for circuit diagrams, operations, and usage of high-voltage IPDs. Keep it at hand for reference.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.