Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What is the definition of “allowable power dissipation”?

The allowable power dissipation is the maximum power dissipation permitted at up to the rated maximum junction temperature (Tj) of 150℃ when the ambient temperature, Ta, is 25℃. The allowable power dissipation should be derated for ambient temperature because it changes with temperature.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.