Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

How does a low-voltage IPD sense temperature for thermal shutdown?

The thermal shutdown temperature is detected by monitoring the forward voltage (VF) of a temperature-sensing diode on a chip.

The forward voltage of the diode has a temperature coefficient of roughly -2 mV/°C. The forward voltage of the temperature-sensing diode is compared with the internal reference voltage, and when the forward voltage falls below the reference voltage because of an increase in temperature, the thermal shutdown threshold is tripped to protect the IPD from excessive temperature.

Temperature-sensing circuit

Figure 1 Temperature-sensing circuit

Thermal shutdown temperature

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.