Is the output status of the sequential circuit such as flip-flops, registers, counters, and one-shot multivibrators determined after the power is turned on?

The output states of flip-flops, registers, counters and one-shot multi-vibrators after power-on are not determinate. (They can be High or Low.)

Generally, the logic state after power-on is initially set by temporarily asserting the CLEAR pin or another pin. This is called a power-on reset. Power-on reset is performed either by a power-on reset circuit that consists of resistors and transistors or by an IC specifically designed for a reset signal.

Related Links

The following documents also contain related information.

Product Lists

Application Notes

A new window will open