Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

For a photocoupler and photorelay incorporating a LED device, in designing equipment, which should be considered: LED life or photodetector life?

 In a photocoupler, deterioration over time of the LED rather than the photodetector is dominant. The optical output of the LED deteriorates as the length of time the LED emits light increases. Therefore, by using data on the deterioration over time of the LED in use, the optical output reduction rate is estimated. In designing circuits, the rate of change of optical output is calculated from the usage environment for the set to be used, and the total light-emitting time, and reflected in the initial value for the LED initial forward current (IF).
For details, also refer to Toshiba Application Note "Basic Characteristics and Application Circuit Design of Transistor Couplers", section 2-4 Design Example for Interface Circuit Using Transistor Coupler.
(https://toshiba.semicon-storage.com/ap-en/design-support/document/application-note.html)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.