Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

Can photorelays be replaced with and used in the same way as mechanical relays? What is the difference, if any?

A mechanical relay consists of mechanical contacts, whereas a photorelay is a semiconductor contact consisting of MOSFETs for output. Because of the above, photorelays have the following benefits compared with mechanical relays:

  • 1.Free from contact wear and thus highly reliable (long life)
  • 2.Small, lightweight and easy to mount
  • 3.High-speed switching (several times faster than mechanical relays)
  • 4.Low power consumption: several mW (compared to approx. 100 mW for mechanical relays)
  • 5.Less bounce noise owing to the absence of mechanical contacts

However, there are disadvantages:

  • a.In contact resistance (ON-state resistance), the difference between metal and semiconductor is too large.
  • b.In the contact open/close capacity (ON-state current), for photorelays, the range that can be covered by one device is very limited.
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.