Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

When controlling a load with a triac coupler, can a load be controlled even if using a rectangular wave power supply at the load side instead of a sinusoidal wave (AC) power supply?

When controlling the turning ON/OFF of a load with a triac coupler, the power supply is intended to be used at a commercial frequency of sinusoidal wave.(50/60Hz). Using a rectangular wave power supply is not recommended, because if doing so, high-frequency components contained in a rectangular wave may cause malfunction.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.