Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What is an RF MOSFET?

MOSFET stands for metal-oxide-semiconductor field-effect transistor. It is a field-oxide transistor with a MOS structure.
Toshiba offers typical single-gate MOS devices with one Gate (G) terminal, and dual-gate MOS devices with two Gate (G) terminals.

This figure explains the symbols of Single Gate MOS and Dual Gate MOS.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.