Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

Does Toshiba support Fujitsu HDDs, which are designed for built-in use?

Toshiba supports Fujitsu HDDs that are within warranty period and designed for built-in use through the manufacturer of your system in which your HDD is installed.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.